External Interface¶
The external interfaces include APIs and callbacks. Only the uGAP APIs are exposed to the application. The application is responsible for registering callbacks and handling them appropriately.
APIs¶
For complete listing of Micro BLE Stack APIs, see Micro BLE Stack API Reference
Callbacks¶
Callbacks are how the TI Micro BLE Stack communicates with the Application. These callbacks are triggered at various events and will contain status or payload depending on the role.
These callbacks should be defined by the Application and registered by passing the structure of callbacks to the role’s initialization function.
Broadcaster Callbacks (BroadcasterCBs)
Observer Callbacks (ObserverCBs)
Connection Monitor Callbacks (MonitorCBs)