GAP Bond Manager and LE Secure Connections

Attention

The CC23xx platform is still under development and some of the features mentioned on this page might not be available yet. Make sure to review the release notes of the SimpleLink Low Power F3 SDK for a complete overview of the features currently supported.

The GAP Bond Manager (GAPBondMgr) is a configurable module that offloads most of the Pairing & Bonding security mechanisms associated with the Security Manager (SM) protocol from the application. The GAPBongMgr executes in the protocol stack task’s context. Table 10. lists the terminology.

Table 10. GAP Bond Manager Terminology

Term

Description

Pairing

The process of generating & exchanging keys. Not to be confused with forming or establishing a BLE connection between two devices.

Encryption

Data is encrypted after pairing, or re-encryption (a subsequent connection where keys are looked up from non-volatile memory).

Association

The pairing method used based on the I/O Capabilities of both devices. For LE devices, Just Works, Numeric Comparison, Passkey Entry and Out-Of-Band are supported.

Authentication

The pairing process using an association method that supports MITM (Man in the Middle) protection.

Bonding

Storing the keys generated during the pairing process in non-volatile memory to use for the next encryption sequence.

Authorization

An additional application level verification in addition to authentication.

OOB

Out of Band. Pairing keys are not exchanged over the air, but rather over some other sources such as serial port or NFC. This provides MITM protection.

MITM

Man in the Middle protection. MITM provides authentication during the pairing process which helps prevent a malicious attacker from impersonating the peer device during the key exchange.

Just Works

Unauthenticated pairing association method where keys are exchanged without MITM protection.

The general process that the GAPBondMgr uses is as follows:

1. The pairing process: exchange keys through the methods described in Selection of Pairing Method.

  1. The encryption process: Encrypt the link using keys Step 1.

  2. The bonding process: store keys in secure flash (Non-Volatile memory).

  3. Reconnecting: Use the keys stored in Non-Volatile memory to encrypt the link.

Tip

Performing all of these steps is not necessary. For example, two devices may choose to pair but not bond.

Security Modes in a Bluetooth LE Connection

The Generic Access Protocol (GAP) layer defines two security modes, along with several security levels per mode.

Security Mode 1 enforces security by means of encryption, and contains four levels:

  • Level 1: No Security (No authentication and no encryption)

  • Level 2: Unauthenticated pairing with encryption

  • Level 3: Authenticated pairing with AES-CCM encryption

  • Level 4: Authenticated LE Secure Connections pairing with encryption using Elliptic Curve Diffie-Hellman P-256 (ECDH) and AES-CCM encryption.

Security Mode 2 enforces security by means of data signing, and contains two levels:

  • Level 1: Unauthenticated pairing with data signing

  • Level 2: Authenticated pairing with data signing

A connection is always established in Security Mode 1, level 1 and can later be upgraded to any other security level. The pairing method chosen determines the actual security mode and level achievable. As discussed in Selection of Pairing Method, the pairing method is selected based on the capabilities of the devices in the connection.

When configured to do so, the BLE5-Stack allows to achieve all the security modes and levels presented, including security mode 1 level 4.

Additional details regarding this topic can be found in [Vol 3], Part C, section §10 of the Bluetooth Core Specifications Version 5.3.

Selection of Pairing Method

Bluetooth Core Specification Version 4.2 added support for the LE Secure Connections feature to enable additional strength to the BLE pairing process. For a detailed description of the algorithms used for LE Secure Connections, see the Security Architecture section ([Vol 1], Part A, Section 5.1) of the Bluetooth Core Specifications Version 5.3. The previous pairing methods used in the Bluetooth Core Specification Versions 4.1 and 4.0 are still available, and are now defined as LE Legacy Pairing. The main difference is that Secure Connection uses Elliptic Curve Diffie-Hellman (ECDH) cryptography, while LE Legacy Pairing does not.

There are four types of pairing methods which are referred to as “Association Models” in the core specification. Each pairing method is described in detail in GAPBondMgr Examples for Different Pairing Methods.

  • Just Works (LE Secure Connections or LE Legacy)

  • Passkey Entry (LE Secure Connections or LE Legacy)

  • Numeric Comparison (LE Secure Connections)

  • Out Of Band (LE Secure Connections or LE Legacy)

Which pairing method is selected, and whether or not pairing will succeed depends on the following parameters from both peer devices during the pairing process:

  • Out Of Band (OOB) set / not set

  • Man In The Middle (MITM) set / not set

  • Input/Output (IO) Capabilities

  • LE Secure Connections supported / not supported

The GAPBondMgr parameters, as they map to the table parameters below are listed here. For more information on these parameters, see BLE Stack API Reference (GAPBondMgr section).

The tables below are from the Selecting Key Generation Method section ([Vol 3], Part H, Section 2.3.5.1) of the Bluetooth Core Specifications Version 5.3. Use these tables to determine which pairing mode is selected for any set of parameters.

If both devices support LE Secure Connections, use Table 11. to decide upon the next step.

Table 11. GAPBondMgr parameters when LE Secure Connections is supported by both devices

Initiator OOB Set

Initiator OOB Not Set

Initiator MITM Set

Initiator MITM Not Set

Responder OOB Set

Use OOB

Use OOB

Responder OOB Not Set

Use OOB

Check MITM

Responder MITN Set

Use IO Capabilities

Use IO Capabilities

Responder MITN Not Set

Use IO Capabilities

Use Just Works

If at least one device does not support LE Secure Connections, use Table 12. to decide upon the next step.

Table 12. GAPBondMgr parameters when LE Secure Connections is not supported by one or both devices.

Initiator OOB Set

Initiator OOB Not Set

Initiator MITM Set

Initiator MITM Not Set

Responder OOB Set

Use OOB

Check MITM

Responder OOB Not Set

Check MITM

Check MITM

Responder MITN Set

Use IO Capabilities

Use IO Capabilities

Responder MITN Not Set

Use IO Capabilities

Use Just Works

If, based on one of the previous tables, IO capabilities are to be used to determine the association model, use Table 13.

Table 13. GAPBondMgr parameters with IO capabilities

Responder

Initiator

Display Only

Display YesNo

Keyboard Only

NoInput NoOutput

Keyboard Display

Display Only

Just Works Unauthenticated

Just Works Unauthenticated

Passkey Entry: Responder displays, Initiator inputs Authenticated

Just Works Unauthenticated

Passkey Entry: Responder displays, Initiator inputs Authenticated

Display YesNo

Just Works Unauthenticated

Just Works (For LE Legacy Pairing) Unauthenticated

Passkey Entry: Responder displays, Initiator inputs Authenticated

Just Works Unauthenticated

Passkey Entry (For LE Legacy Pairing) Responder displays Initiator inputs Authenticated

Numeric Comparison (For LE Secure Connections) Authenticated

Numeric Comparison (For LE Secure Connections) Authenticated

Keyboard Only

Passkey Entry: Initiator displays, Responder inputs Authenticated

Passkey Entry: Initiator displays, Responder inputs Authenticated

Passkey Entry: Initiator displays, Responder inputs Authenticated

Just Works Unauthenticated

Passkey Entry: Initiator displays, Responder inputs Authenticated

NoInput NoOutput

Just Works Unauthenticated

Just Works Unauthenticated

Just Works Unauthenticated

Just Works Unauthenticated

Just Works Unauthenticated

Keyboard Display

Passkey Entry: Initiator displays, Responder inputs Authenticated

Passkey Entry (For LE Legacy Pairing) Initiator displays Responder inputs Authenticated

Passkey Entry: Responder displays, Initiator inputs Authenticated

Just Works Unauthenticated

Passkey Entry (For LE Legacy Pairing) Initiator displays Responder inputs Authenticated

Numeric Comparison (For LE Secure Connections) Authenticated

Numeric Comparison (For LE Secure Connections) Authenticated

Using GAPBondMgr

This section describes what the application must do to configure, start, and use the GAPBondMgr. The GAPBondMgr is defined in gapbondmgr.c and gapbondmgr.h. BLE Stack API Reference (GAPBondMgr section) describes the full API including commands, configurable parameters, events, and callbacks.

The GAPBondMgr is enabled by default using SysConfig in all BLE5-Stack projects, with the exception of host_test. The following steps are provided for reference.

The general steps to use the GAPBondMgr module are as follows:

1. Configure the stack to include GAPBondMgr functionality by defining the following in build_config.opt in the project:

  • -DGAP_BOND_MGR

Note

GAPBondMgr is included by default using sysConfig tool in most of the examples except host_test. Thus step 1 is only applicable for host_test example.

2. If using LE Secure Connections, the PDU size must be >= 69. This can be set by defining the following preprocessor symbol in the application project: MAX_PDU_SIZE=69.

Note

MAX_PDU_SIZE is set to 69 by default using sysConfig tool in most of the examples except host_test. This step is only applicable for host_test example.

3. Configure the GAPBondMgr by initializing its parameters as desired. GAPBondMgr configuration parameters are not persistent and must be configured after the device is reset. See BLE Stack API Reference (GAPBondMgr section) for a complete list of parameters with functionality described. There are examples of this for the various pairing/bonding modes in GAPBondMgr Examples for Different Pairing Methods.

4. Register application callbacks with the GAPBondMgr, so that the application can communicate with the GAPBondMgr and be notified of events.

Listing 80. ble_stack_api.c bleStack_initGapBond - Initialize GapBondMgr
// Start Bond Manager and register callback
VOID GAPBondMgr_Register((gapBondCBs_t *)bleApp_bondMgrCBs);

Here bleApp_bondMgrCBs is defined as a structure containing the GAPBondMgr Callbacks. A passcode callback function is mandatory.

Listing 81. bleapputil_init.c Register callback
// GAP Bond Manager Callbacks
gapBondCBs_t BLEAppUtil_bondMgrCBs =
{
    BLEAppUtil_passcodeCB, // Passcode callback
    BLEAppUtil_pairStateCB // Pairing/Bonding state Callback
};

The above excerpt comes from the Basic BLE framework. It is not recommended to modify this file but rather to register for an application callback using the provided framework. In short, take a look at this excerpt from app_pairing.c that defines an EventHandler function using the BLEAppUtil framework.

BLEAppUtil_EventHandler_t pairingPasscodeHandler =
{
    .handlerType    = BLEAPPUTIL_PASSCODE_TYPE,
    .pEventHandler  = Pairing_passcodeHandler
};

BLEAppUtil_EventHandler_t PairingPairStateHandler =
{
    .handlerType    = BLEAPPUTIL_PAIR_STATE_TYPE,
    .pEventHandler  = Pairing_pairStateHandler,
    .eventMask      = BLEAPPUTIL_PAIRING_STATE_STARTED |
                      BLEAPPUTIL_PAIRING_STATE_COMPLETE |
                      BLEAPPUTIL_PAIRING_STATE_ENCRYPTED |
                      BLEAPPUTIL_PAIRING_STATE_BOND_SAVED,
};

5. Once the GAPBondMgr is configured, it operates mostly autonomously from the perspective of the application. When a connection is established, the GAPBondMgr manages pairing and bonding depending on the configuration parameters set during initialization. It also communicates with the application as needed through the defined callbacks.

A few parameters can be set and functions can be called asynchronously at any time from the application. See BLE Stack API Reference (GAPBondMgr section) for more information.

Most communication between the GAPBondMgr and the application at this point occurs through the callbacks which were registered in Step 4. Figure 82. is a flow diagram example of the GAPBondMgr notifying the application that pairing has been completed. The same method occurs for various other events and will be expanded upon in the following section.

@startuml
  participant Application
  participant BLEAppUtil as "BLE Application Framework"
  participant Gapbondmgr as "GAPBondMgr"
  participant BLEStack as "BLE Stack"

  BLEStack -> Gapbondmgr : GAP_AUTHENTICATION_\nCOMPLETE_EVENT
  Gapbondmgr -> BLEAppUtil : Pairing state callback
  BLEAppUtil -> BLEAppUtil : BLEAppUtil_pairStateCB
  rnote over "BLEAppUtil"
    BLEAPPUTIL_EVT_PAIRING_STATE_CB
  end note
  BLEAppUtil -> BLEAppUtil: BLEAppUtil_processPairStateMsg
  rnote over "Application"
    BLEAPPUTIL_PAIR_STATE_TYPE
  end note
  BLEAppUtil -> Application: PairingPairStateHandler
  rnote over "Application"
    BLEAPPUTIL_PAIRING_STATE_COMPLETE
  end note

@enduml

Figure 82. GapBondMgr Callback Example.

GAPBondMgr Examples for Different Pairing Methods

This section provides message diagrams for the types of security that can be implemented. These modes assume acceptable I/O capabilities are available for the security mode, and that the selection of whether or not to support LE Secure Connections allows for the pairing method. See the Selection of Pairing Method on how these parameters affect pairing. These examples only consider the pairing aspect. Bonding can be added to each type of pairing in the same manner and is shown in the next section.

Caution

The code snippets here are not complete functioning examples, and are only intended for illustration purposes.

Warning

It is not allowed to set MITM to TRUE while IO capability is set to GAPBOND_IO_CAP_NO_INPUT_NO_OUTPUT since these two conflict each other.

Disabling Pairing

With pairing mode set to GAPBOND_PAIRING_MODE_NO_PAIRING, the BLE5-Stack automatically rejects any attempt at pairing. Configure the GAPBondMgr as follows to disable pairing:

// Pairing is not allowed
uint8_t pairMode = GAPBOND_PAIRING_MODE_NO_PAIRING;
GAPBondMgr_SetParameter(GAPBOND_PAIRING_MODE, sizeof(uint8_t), &pairMode);

Enabling Pairing

To start or allow the pairing process after a connection is formed, the GAPBondMgr can be configured to automatically request pairing or wait for pairing request from a peer device. The actual behavior depends on the device’s GAP role (Central or Peripheral) and the setting of the GAPBondMgr pairing mode (GAPBOND_PAIRING_MODE).

To initiate the pairing process on Peripheral role devices, GAPBOND_PAIRING_MODE_INITIATE will send a Slave Security Request shortly after the GAPBondMgr is informed that the connection is formed. For Central role devices, GAPBOND_PAIRING_MODE_INITIATE will send a Pairing Request or request the Link Layer to encrypt the link if the device has previously paired/bonded:

// Initiate pairing request
uint8_t pairMode = GAPBOND_PAIRING_MODE_INITIATE;
GAPBondMgr_SetParameter(GAPBOND_PAIRING_MODE, sizeof(uint8_t), &pairMode);

The Peripheral can be configured to wait for a Pairing Request from the Central when the pairing mode is set to GAPBOND_PAIRING_MODE_WAIT_FOR_REQ. When this pairing mode is selected, the GAPBondMgr will automatically respond with a Pairing Response based on other GAPBondMgr configured parameters.

// Wait for a pairing request
uint8_t pairMode = GAPBOND_PAIRING_MODE_WAIT_FOR_REQ;
GAPBondMgr_SetParameter(GAPBOND_PAIRING_MODE, sizeof(uint8_t), &pairMode);

Tip

When pairing with smartphone Central devices, it is recommended to use GAPBOND_PAIRING_MODE_WAIT_FOR_REQ as undefined behavior may occur when a Slave Security Request is sent by the Peripheral. Both iOS and Android will initiate pairing when the peripheral responds with an Insufficient Authentication error response when a GATT secure characteristic is accessed.

Pairing can also be enabled by utilizing GAPBondMgr_Pair(). This API can be used to start the pairing process when pairing is not started automatically by the GAPBondMgr. An example use case of this API is to be able to start pairing from the application. This API can also be used to re-pair after initial pairing has occurred. An example use case of this is if pairing requirements have changed and need to be updated. See BLE Stack API Reference GAPBondMgr section for more information on the function.

bStatus_t stat = GAPBondMgr_Pair(connHandle);

LE Secure Connections

LE Secure Connections is enabled by default in BLE5-Stack. If you don’t want to use LE Secure Connections, set the GAPBOND_SECURE_CONNECTION variable to GAPBOND_SECURE_CONNECTION_NONE during the GAPBondMgr initialization.

uint8_t gapbondSecure = GAPBOND_SECURE_CONNECTION_NONE;
GAPBondMgr_SetParameter(GAPBOND_SECURE_CONNECTION, sizeof(uint8_t), &gapbondSecure);

It is important when trying to decipher over-the-air sniffer logs with LE Secure Connections enabled, you need to use a specific “debug” key as defined by Vol 3 Part H section 2.3.5.6.1 of the Bluetooth Core Specifications Version 5.3. In the BLE5-Stack, this key is enabled using SysConfig, by checking ‘ECC Debug Keys’ under BLE, Bond Manager (see Bond Manager). When either the initiating or non-initiating device uses this specific debug key, it enables over-the-air sniffer equipment that supports LE Secure Connections to determine the LTK and therefore monitor/decrypt encrypted traffic throughout the connection.

LESC Limitations & Recommendations

LE Secure Connections uses an ECDH public-private key pair as part of the pairing process. See Selection of Pairing Method and the LE Secure Connections Pairing Phase 2 section of the Bluetooth Core Specifications Version 5.3 for more information about how these keys and how they are used in the pairing process.

To summarize, as part of LESC pairing Phase 1 each device will generate its own ECDH public-private key pair. As part of LESC pairing Phase 2 each device will compute the Diffie-Hellman (DH) Key based on the public keys that are exchanged.

ECC public-private and DH key generation is implemented by the ECDH TI-RTOS7 driver for the Private Key Accelerator (PKA) on the CC23xx. These routines are blocking by nature and take around 136.5ms to execute. During LESC pairing, the ECDH driver will be accessed twice by the link layer (LL) once to generate the public/private key pair and again to generate the DH key. This means the stack OSAL tasks will be blocked for around 136.5ms twice during pairing. However, the user application task will be able to run at this time.

Because of this, TI recommends the following when using LESC:

  • Supervision timeout >= 140ms

To alleviate the amount of blocking required, the user application can generate the public-private key pair ahead of the pairing process, or it can define when the keys should be recycled by using the following parameters of the GapBondMgr. These options are mutually exclusive, as generation of keys by the application bypasses the recycle parameter. To truly minimize the affect of ECC on the BLE connection, perform ECC before any connections are established.

Authentication Pairing Only

For users that want the pairing method results in a key generation that provides Authenticated MITM protection only, they can achieve that by doing the following.

uint8_t ioCap = GAPBOND_IO_CAP_KEYBOARD_DISPLAY;
uint8_t mitm = TRUE;
uint8_t authenPairingOnly = TRUE;

// Only certain combinations of IO capability will result
// authenticad pairing mode. Here we use GAPBOND_IO_CAP_KEYBOARD_DISPLAY
// as code example to make sure whichever IO capability other than NoInput
// NoOutput the peer device has will result in an authenticated link
GAPBondMgr_SetParameter(GAPBOND_IO_CAPABILITIES, sizeof(uint8_t), &ioCap);

// For authenticated pairing, MITM has to be set to TRUE
GAPBondMgr_SetParameter( GAPBOND_MITM_PROTECTION, sizeof (uint8_t), &mitm);

// Enable authentication only pairing
GAPBondMgr_SetParameter( GAPBOND_AUTHEN_PAIRING_ONLY, sizeof (uint8_t), &authenPairingOnly);

Upon setting GAPBOND_AUTHEN_PAIRING_ONLY to true, if the peer device’s IO capability can not result in authenticated link, the BLE5-Stack will reject the pairing and return error code SMP_PAIRING_FAILED_AUTH_REQ.

 @startuml

  participant Application
  participant BLEAppUtil as "BLE Application Framework"
  participant Gapbondmgr as "GAPBondMgr"
  participant BLEStack as "BLE Stack"

  BLEStack -> Gapbondmgr : GAP_LINK_ESTABLISHED_EVENT
  Gapbondmgr -> BLEStack : GAPBondMgr_LinkEst()
  Gapbondmgr -> BLEStack : GAP_Authenticate()
  BLEStack -->] : Pairing req
  Gapbondmgr -> BLEAppUtil : BLEAppUtil_pairStateCB
  BLEAppUtil -> Application : PairingPairStateHandler
  rnote over Application
  BLEAPPUTIL_PAIRING_
  STATE_STARTED
  end note
  BLEStack <--] : Pairing rsp
    rnote over BLEStack
      Base on the IO capability, MITM, OOB setting of both devices,
      STACK needs to sort out whether this results to Just Work pairing.
    end note

  group if the pairing method (Just Work) can not fulfill Authentication MITM protection

    BLEStack -->] : End pairing
    BLEStack -> Gapbondmgr : GAP_AUTHENTICATION_\nCOMPLETE_EVENT
    Gapbondmgr -> BLEAppUtil : BLEAppUtil_pairStateCB
    BLEAppUtil -> Application: PairingPairStateHandler
    rnote over Application
      BLEAPPUTIL_PAIRING_STATE_COMPLETE
      SMP_PAIRING_FAILED_AUTH_REQ
    end note
  end
@enduml

Figure 83. Authentication Only Pairing.

For more information regarding which pairing mode results authenticated link, please refer Table 13.

Just Works Pairing

Just Works pairing allows encryption without authentication and is vulnerable to MITM attacks. Just Works pairing can be LE Legacy or LE Secure Connections pairing. The GAPBondMgr does not need any additional input from the application for Just Works pairing. Configure the GAPBondMgr for Just Works pairing as follows.

uint8_t mitm = FALSE;
GAPBondMgr_SetParameter( GAPBOND_MITM_PROTECTION, sizeof (uint8_t), &mitm);

Figure 84. describes the interaction between the GAPBondMgr and the application for Just Works pairing. As shown, the application receives a GAPBOND_PAIRING_STATE_STARTED event once the pairing request has been sent, and a GAPBOND_PAIRING_STATE_COMPLETE event once the pairing process has been completed. At this time, the link is encrypted.

 @startuml

  participant Application
  participant BLEAppUtil as "BLE Application Framework"
  participant Gapbondmgr as "GAPBondMgr"
  participant BLEStack as "BLE Stack"

  BLEStack -> Gapbondmgr : GAP_LINK_ESTABLISHED_EVENT
  Gapbondmgr -> BLEStack : GAPBondMgr_LinkEst()
  Gapbondmgr -> BLEStack : GAP_Authenticate()
  BLEStack -->] : Pairing req
  Gapbondmgr -> BLEAppUtil : BLEAppUtil_pairStateCB
  BLEAppUtil -> Application : PairingPairStateHandler
  rnote over Application
  BLEAPPUTIL_PAIRING_
  STATE_STARTED
  end note

  BLEStack -->] : Encryption req
  BLEStack <--] : Encryption rsp
  BLEStack -> Gapbondmgr : GAP_AUTHENTICATION_\nCOMPLETE_EVENT
  Gapbondmgr -> BLEAppUtil : BLEAppUtil_pairStateCB
  BLEAppUtil -> Application: PairingPairStateHandler
  rnote over Application
    BLEAPPUTIL_PAIRING_
    STATE_COMPLETE
  end note
@enduml

Figure 84. Just Works Pairing.

Passcode Entry

Passkey entry is a type of authenticated pairing that can prevent man in the middle (MITM) attacks. It can be used with either LE Legacy pairing or Secure Connections pairing. In this pairing method, one device displays a 6-digit passcode, and the other device enters the passcode. As described in Selection of Pairing Method, the IO capabilities decide which device performs which role. The passcode callback registered with the GAPBondMgr when it was started is used to enter or display the passcode. The following is an example of initiating Passcode Entry pairing where the passcode is displayed.

  1. Define passcode callback

Listing 82. Define passcode callback.
  BLEAppUtil_EventHandler_t pairingPasscodeHandler =
  {
      .handlerType    = BLEAPPUTIL_PASSCODE_TYPE,
      .pEventHandler  = Pairing_passcodeHandler
  };

  /*********************************************************************
  * @fn      Pairing_passcodeHandler
  *
  * @brief   The purpose of this function is to handle passcode data
  *          that rise from the GAPBondMgr and were registered
  *          in @ref BLEAppUtil_RegisterGAPEvent
  *
  * @param   pMsgData - pointer to message data.
  *
  * @return  none
  */
  void Pairing_passcodeHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
  {
      BLEAppUtil_PasscodeData_t *pData = (BLEAppUtil_PasscodeData_t *)pMsgData;

      // Send passcode response
      GAPBondMgr_PasscodeRsp(pData->connHandle, SUCCESS, B_APP_DEFAULT_PASSCODE);
  }
  1. Configure GAPBondMgr

Listing 83. Configure GAPBondMgr for MITM.
uint8_t pairMode = GAPBOND_PAIRING_MODE_INITIATE;
uint8_t mitm = TRUE;
GAPBondMgr_SetParameter(GAPBOND_PAIRING_MODE, sizeof(uint8_t), &pairMode);
GAPBondMgr_SetParameter(GAPBOND_MITM_PROTECTION, sizeof(uint8_t), &mitm);
  1. Process passcode callback and send the response to the stack.

Listing 84. Process passcode and send the response.
//! BLE Default Passcode
#define B_APP_DEFAULT_PASSCODE                    123456

void Pairing_passcodeHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
{
    BLEAppUtil_PasscodeData_t *pData = (BLEAppUtil_PasscodeData_t *)pMsgData;

  // Display passcode to user
  if(pData->uiOutputs)
  {
      Display_printf(dispHandle, dispIndex, 0, "#%5d    Passcode: %d", dispIndex, B_APP_DEFAULT_PASSCODE); dispIndex++;
  }

  // Send passcode response
  GAPBondMgr_PasscodeRsp(connHandle , SUCCESS, B_APP_DEFAULT_PASSCODE);
}

Depending on the uiInputs and uiOutputs returned from the GAPBondMgr, the passcode must either be entered or displayed. The passcode is then sent to the GAPBondMgr using GAPBondMgr_PasscodeRsp(), so that pairing can continue. In this case, the password is statically set to 123456. In a real product, the password will likely be randomly generated, and the device must expose a way for the user to enter the passcode, then send it to the GAPBondMgr using GAPBondMgr_PasscodeRsp(). An example interaction between the GAPBondMgr and the application is shown in Figure 85..

 @startuml
  participant Application
  participant BLEAppUtil as "BLE Application Framework"
  participant Gapbondmgr as "GAPBondMgr"
  participant BLEStack as "BLE Stack"

  BLEStack -> Gapbondmgr : GAP_LINK_ESTABLISHED_EVENT
  Gapbondmgr -> BLEStack : GAPBondMgr_LinkEst()
  Gapbondmgr -> BLEStack : GAP_Authenticate()
  BLEStack -->] : Pairing req

  Gapbondmgr -> BLEAppUtil : BLEAppUtil_pairStateCB
  rnote over "BLEAppUtil"
    BLEAPPUTIL_EVT_PAIRING_STATE_CB
  end note
  BLEAppUtil -> BLEAppUtil: BLEAppUtil_processPairStateMsg
  rnote over "Application"
    BLEAPPUTIL_PAIR_STATE_TYPE
  end note
  BLEAppUtil -> Application: PairingPairStateHandler
  rnote over "Application"
    BLEAPPUTIL_PAIRING_STATE_STARTED
  end note

  BLEStack -> Gapbondmgr : GAP_PASSKEY_NEEDED_\nEVENT
  Gapbondmgr -> BLEAppUtil: BLEAppUtil_passcodeCB
  BLEAppUtil -> Application: Pairing_passcodeHandler
  [--> Application : Enter or display\npasscode
  Application -> Gapbondmgr : GAPBondMgr_PasscodeRsp()
  Gapbondmgr -> BLEStack : GAP_PasscodeUpdate()
  BLEStack -->] : Encryption req
  BLEStack <--] : Encryption rsp
  BLEStack -> Gapbondmgr : GAP_AUTHENTICATION_\nCOMPLETE_EVENT
  Gapbondmgr -> BLEAppUtil: BLEAppUtil_pairStateCB
  BLEAppUtil -> Application : PairingPairStateHandler

  rnote over Application
  BLEAPPUTIL_PAIRING_
  STATE_COMPLETE
  end note
@enduml

Figure 85. Interaction Between the GAPBondMgr and the Application when exchanging a passcode.

Numeric Comparison

Numeric comparison is a type of authenticated pairing that protects from MITM attacks. It is only possible as a LE Secure Connections pairing; not LE legacy. For numeric comparison pairing, both devices display a 6-digit code. Each device must then indicate, through a button press or some other Yes-No input, whether the codes match. The passcode callback registered with the GAPBondMgr when it was started is used to display the 6-digit code. The following is an example of initiating Numeric Comparison pairing where the passcode is displayed. The IO capabilities must be set appropriately to select numeric comparison (that is, Display/Yes-No on both sides).

  1. Define passcode callback to display code.

Listing 85. Define passcode callback to display code.
 1BLEAppUtil_EventHandler_t pairingPasscodeHandler =
 2{
 3    .handlerType    = BLEAPPUTIL_PASSCODE_TYPE,
 4    .pEventHandler  = Pairing_passcodeHandler
 5};
 6
 7/*********************************************************************
 8* @fn      Pairing_passcodeHandler
 9*
10* @brief   The purpose of this function is to handle passcode data
11*          that rise from the GAPBondMgr and were registered
12*          in @ref BLEAppUtil_RegisterGAPEvent
13*
14* @param   pMsgData - pointer to message data.
15*
16* @return  none
17*/
18void Pairing_passcodeHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
19{
20    BLEAppUtil_PasscodeData_t *pData = (BLEAppUtil_PasscodeData_t *)pMsgData;
21
22    // Send passcode response
23    GAPBondMgr_PasscodeRsp(pData->connHandle, SUCCESS, B_APP_DEFAULT_PASSCODE);
24}
  1. Configure GAPBondMgr

Listing 86. Configure GAPBondMgr For LE Secure Connections + Authentication.
1uint8_t pairMode = GAPBOND_PAIRING_MODE_WAIT_FOR_REQ;
2uint8_t scMode = GAPBOND_SECURE_CONNECTION_ONLY;
3uint8_t mitm = TRUE;
4uint8_t ioCap = GAPBOND_IO_CAP_DISPLAY_YES_NO;
5
6GAPBondMgr_SetParameter(GAPBOND_IO_CAPABILITIES, sizeof(uint8_t), &ioCap);
7GAPBondMgr_SetParameter(GAPBOND_PAIRING_MODE, sizeof(uint8_t), &pairMode);
8GAPBondMgr_SetParameter(GAPBOND_MITM_PROTECTION, sizeof(uint8_t), &mitm);
9GAPBondMgr_SetParameter(GAPBOND_SECURE_CONNECTION, sizeof(uint8_t), &scMode);
  1. Process passcode callback and display code.

Listing 87. Process passcode callback and display code.
 1void Pairing_passcodeHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
 2{
 3    BLEAppUtil_PasscodeData_t *pData = (BLEAppUtil_PasscodeData_t *)pMsgData;
 4
 5  // Display passcode to user
 6  if(pData->uiOutputs)
 7  {
 8      Display_printf(dispHandle, dispIndex, 0, "#%5d    Passcode: %d", dispIndex, B_APP_DEFAULT_PASSCODE); dispIndex++;
 9  }
10
11  // Send passcode response
12  GAPBondMgr_PasscodeRsp(connHandle , SUCCESS, B_APP_DEFAULT_PASSCODE);
13}
  1. Accept Yes-No input from user and send response to GAPBondMgr.

Listing 88. Accept Yes-No input from user and send response to GAPBondMgr.
1//example of "Yes" input via button press
2if (btn-pressed)
3{
4  //Send response to indicate that code matches
5  GAPBondMgr_PasscodeRsp(connHandle, SUCCESS, TRUE);
6  return;
7}

In this case, the third parameter of GAPBondMgr_PasscodeRsp, which usually accepts a passcode, is overloaded to send TRUE to the stack to indicate that the codes match and to continue with pairing. The process of numeric comparison is illustrated in Figure 86.

 @startuml
  participant Application
  participant BLEAppUtil as "BLE Application Framework"
  participant Gapbondmgr as "GAPBondMgr"
  participant BLEStack as "BLE Stack"

  BLEStack -> Gapbondmgr : GAP_LINK_ESTABLISHED_EVENT
  Gapbondmgr -> BLEStack : GAPBondMgr_LinkEst()
  Gapbondmgr -> BLEStack : GAP_Authenticate()
  BLEStack -->] : Pairing req

  Gapbondmgr -> BLEAppUtil : BLEAppUtil_pairStateCB
  rnote over "BLEAppUtil"
    BLEAPPUTIL_EVT_PAIRING_STATE_CB
  end note
  BLEAppUtil -> BLEAppUtil: BLEAppUtil_processPairStateMsg
  rnote over "Application"
    BLEAPPUTIL_PAIR_STATE_TYPE
  end note
  BLEAppUtil -> Application: PairingPairStateHandler
  rnote over "Application"
    BLEAPPUTIL_PAIRING_STATE_STARTED
  end note

  BLEStack -> Gapbondmgr : GAP_PASSKEY_NEEDED_\nEVENT
  Gapbondmgr -> BLEAppUtil: BLEAppUtil_passcodeCB
  BLEAppUtil -> Application: Pairing_passcodeHandler
  [<-- Application : Display code
  [--> Application : Codes match

  Application -> Gapbondmgr : GAPBondMgr_PasscodeRsp()
  Gapbondmgr -> BLEStack : GAP_PasscodeUpdate()

  BLEStack -->] : Encryption req
  BLEStack <--] : Encryption rsp
  BLEStack -> Gapbondmgr : GAP_AUTHENTICATION_\nCOMPLETE_EVENT
  Gapbondmgr -> BLEAppUtil: BLEAppUtil_pairStateCB
  BLEAppUtil -> Application : PairingPairStateHandler

  rnote over Application
  BLEAPPUTIL_PAIRING_
  STATE_COMPLETE
  end note
@enduml

Figure 86. Numeric Comparison.

Out of Band Pairing

Out of Band is a feature that allows two devices to send authentication information over a communication channel that is out of the band of the device, e.g. by NFC. The purpose is to allow two devices with no input or output capabilities to create an authenticated pairing. This happens by sending three authentication parameters: device address, random number and confirm value.

The main purpose of OOB authentication is to protect against MITM attacks. The idea is to generate a key on one device. (This can be the initiator or the responder.) Then the OOB data is communicated to the other device by some other means of communication than Bluetooth LE protocol.

The OOB data is generated at runtime. This can be done using elliptic-curve cryptography (ECC) or not. In this example we will use ECC to generate a key. To generate OOB data with a central application follow these steps:

  1. Create gapBondOOBData_t variables, one for the local OOB data and one for the remote device’s data:

// This is needed for the device that generates OOB data
gapBondOOBData_t localOobData;
// This is needed to store the OOB data this device receives
gapBondOOBData_t remoteOobData;
  1. Define the pair state callback

 1BLEAppUtil_EventHandler_t PairingPairStateHandler =
 2{
 3    .handlerType    = BLEAPPUTIL_PAIR_STATE_TYPE,
 4    .pEventHandler  = Pairing_pairStateHandler,
 5    .eventMask      = BLEAPPUTIL_PAIRING_STATE_STARTED |
 6                      BLEAPPUTIL_PAIRING_STATE_COMPLETE |
 7                      BLEAPPUTIL_PAIRING_STATE_ENCRYPTED |
 8                      BLEAPPUTIL_PAIRING_STATE_BOND_SAVED |
 9                      BLEAPPUTIL_GENERATE_ECC_DONE //This modification is required below
10};
  1. To generate OOB data with ECC keys, you need to call GAPBondMgr_GenerateEccKeys() prior to GAPBondMgr_SCGetLocalOOBParameters(). After calling GAPBondMgr_GenerateEccKeys(), once the ECC keys are ready, the BLE5-Stack will send GAPBOND_GENERATE_ECC_DONE event to application and the event should be processed under pair state callback.

    Then application can call GAPBondMgr_SCGetLocalOOBParameters() to obtain OOB data which is generated using the ECC Keys. The OOB data can then be extracted. The example code below illustrate how to extract the OOB data.

    Warning

    The GAPBondMgr_GenerateEccKeys() and GAPBondMgr_SCGetLocalOOBParameters() can be called either before and after the connection is established. But these need to be called before the pairing started. In this case, we call both functions before the connection is established.

    Listing 89. App_StackInitDoneHandler Generate ECC keys.
    1// Generate ECC Keys
    2GAPBondMgr_GenerateEccKeys();
    
    Listing 90. app_pairing.c:: Pairing_pairStateHandler:: BLEAPPUTIL_GENERATE_ECC_DONE: Generate OOB data after ECC keys are ready.
     1/*********************************************************************
     2* @fn      Pairing_pairStateHandler
     3*
     4* @brief   The purpose of this function is to handle pairing state
     5*          events that rise from the GAPBondMgr and were registered
     6*          in @ref BLEAppUtil_RegisterGAPEvent
     7*
     8* @param   event - message event.
     9* @param   pMsgData - pointer to message data.
    10*
    11* @return  none
    12*/
    13void Pairing_pairStateHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
    14{
    15    BLEAppUtil_PairStateData_t *pairStateMsg = (BLEAppUtil_PairStateData_t *)pMsgData;
    16    switch(event)
    17    {
    18      //.
    19      //.
    20      //.
    21        case BLEAPPUTIL_GENERATE_ECC_DONE:
    22        {
    23          if(pairStateMsg->status == SUCCESS)
    24          {
    25            GAPBondMgr_SCGetLocalOOBParameters(&localOobData);
    26            uint8_t i;
    27            for (i = 0; i < KEYLEN; i++)
    28            {
    29                Display_printf(dispHandle, dispIndex, 0,"#%5d    OOB data confirm[%d]: %d", dispIndex, i, localOobData.confirm[i]); dispIndex++;
    30                Display_printf(dispHandle, dispIndex, 0,"#%5d    OOB data rand[%d]: %d", dispIndex, i, localOobData.rand[i]); dispIndex++;
    31            }
    32          }
    33          break;
    34        }
    35        default:
    36        {
    37            break;
    38        }
    39    }
    40}
    

    Note

    If GAPBondMgr_GenerateEccKeys() is not called before GAPBondMgr_SCGetLocalOOBParameters(), the OOB data will be generated without ECC.

  2. After the OOB data is generated, the device needs to send it over to the peer device using any other medium for example NFC or wired solutions(E.g. UART, SPI, LIN, CAN…etc). The device which has received the OOB data (not the one that generated it) should set the GAPBOND_OOB_ENABLED parameter to true. If both devices have generated and shared their OOB data both should set the flag. In this case we will only set the flag on the peripheral device.

    uint8_t oobEnabled = TRUE;
    
    GAPBondMgr_SetParameter(GAPBOND_OOB_ENABLED, sizeof(uint8_t), &oobEnabled);
    
  3. Perform OOB communication, i.e. communicate the data in localOobData to the responder device. For simplicity, in this example the central device will display the data thus it can be hard coded on the peripheral device.

Listing 91. App_StackInitDoneHandler The OOB data is hard coded on the peripheral device.
 1uint8_t oobEnabled = TRUE;
 2GAPBondMgr_SetParameter(GAPBOND_OOB_ENABLED, sizeof(uint8_t), &oobEnabled);
 3remoteOobData.confirm[0] = 204;
 4remoteOobData.confirm[1] = 29;
 5remoteOobData.confirm[2] = 240;
 6remoteOobData.confirm[3] = 154;
 7remoteOobData.confirm[4] = 141;
 8remoteOobData.confirm[5] = 40;
 9remoteOobData.confirm[6] = 132;
10remoteOobData.confirm[7] = 41;
11remoteOobData.confirm[8] = 156;
12remoteOobData.confirm[9] = 106;
13remoteOobData.confirm[10] = 91;
14remoteOobData.confirm[11] = 230;
15remoteOobData.confirm[12] = 11;
16remoteOobData.confirm[13] = 88;
17remoteOobData.confirm[14] = 117;
18remoteOobData.confirm[15] = 104;
19remoteOobData.rand[0] = 56;
20remoteOobData.rand[1] = 242;
21remoteOobData.rand[2] = 38;
22remoteOobData.rand[3] = 152;
23remoteOobData.rand[4] = 189;
24remoteOobData.rand[5] = 78;
25remoteOobData.rand[6] = 164;
26remoteOobData.rand[7] = 36;
27remoteOobData.rand[8] = 153;
28remoteOobData.rand[9] = 82;
29remoteOobData.rand[10] = 167;
30remoteOobData.rand[11] = 190;
31remoteOobData.rand[12] = 140;
32remoteOobData.rand[13] = 235;
33remoteOobData.rand[14] = 207;
34remoteOobData.rand[15] = 93;
35GAPBondMgr_SCSetRemoteOOBParameters(&remoteOobData, 1);

The process of aforementioned OOB pairing example is illustrated in Figure 87. For simplicity, the BLEAppUtil framework layer is not shown. Remember to use the application defined callbacks inside app_pairing.c as shown in the above sections.

@startuml

    participant cen_app as "Central\nApplication"
    participant cen_gapbondmgr as "Central\nGapbondmgr"
    participant cen_blestack as "Central\nBLE-Stack"

    participant per_blestack as "Peripheral\nBLE-Stack"
    participant per_gapbondmgr as "Peripheral\nGapbondmgr"
    participant per_app as "Peripheral\nApplication"

    cen_app -> cen_gapbondmgr : Generate ECC keys
    cen_gapbondmgr -> cen_blestack : Generate ECC keys

    ==ECC Keys are ready ==
    cen_gapbondmgr -> cen_app : Pairing state callback
    rnote over cen_app
      GAPBOND_GENERATE_
      ECC_DONE
    end note

    cen_app -> cen_gapbondmgr : Get local OOB parameters
    cen_gapbondmgr -> cen_blestack : Compute confirm and rand values
    cen_app -> per_app : Sending OOB data through either NFC or other wired protocol

    == Once peripheral receives OOB data ==
    per_app -> per_app : Set GAPBOND_OOB_ENABLED to true

    == After connection has established ==

    cen_gapbondmgr -> cen_blestack : GAPBondMgr_LinkEst()
    cen_gapbondmgr -> cen_blestack : GAP_Authenticate()
    cen_blestack --> per_blestack : Pairing req
    per_blestack --> cen_blestack : Pairing rsp
    cen_gapbondmgr -> cen_app : Pairing state callback

    rnote over cen_app
    GAPBOND_PAIRING_
    STATE_STARTED
    end note

    per_gapbondmgr -> per_app : Pairing state callback
    rnote over per_app
    GAPBOND_PAIRING_
    STATE_STARTED
    end note

    cen_blestack --> per_blestack : Encryption req
    cen_blestack <-- per_blestack : Encryption rsp
    cen_blestack -> cen_gapbondmgr : GAP_AUTHENTICATION_\nCOMPLETE_EVENT
    cen_gapbondmgr -> cen_app : Pairing state callback
    per_blestack -> per_gapbondmgr : GAP_AUTHENTICATION_\nCOMPLETE_EVENT
    per_gapbondmgr -> per_app : Pairing state callback
    rnote over cen_app
      GAPBOND_PAIRING_
      STATE_COMPLETE
    end note

    rnote over per_app
      GAPBOND_PAIRING_
      STATE_COMPLETE
    end note
@enduml

Figure 87. Out of Band Pairing

GAPBondMgr Examples for Manipulating Bonding

GAPBondMgr offers various functions to help users to:

  1. Enable bonding

  2. Extract bonding information

  3. Import bonding information to NV

Enable Bonding

Bonding can enabled or disabled for any type of pairing through the GAPBOND_BONDING_ENABLED parameter, and occurs after the pairing process is complete. To enable bonding, configure the GAPBondMgr as follows:

uint8_t bonding = TRUE;
GAPBondMgr_SetParameter(GAPBOND_BONDING_ENABLED, sizeof(uint8_t), &bonding);

With bonding enabled, the GAPBondMgr stores the long-term key transferred during the pairing process to NV. See GAPBondMgr and NV for more information. After this is completed, the application is notified through the GAPBOND_PAIRING_STATE_COMPLETE event. GAPBOND_PAIRING_STATE_BOND_SAVED is only passed to the application pair state callback when initially connecting, pairing, and bonding. For future connections to a bonded device, the security keys are loaded from NV, thus skipping the pairing process. In this case, only GAPBOND_PAIRING_STATE_BONDED is passed to the application pair state callback. This is illustrated in Figure 88.

 @startuml

  participant Application
  participant Gapbondmgr as "GAPBondMgr"
  participant BLEStack as "BLE Stack"

  BLEStack -> Gapbondmgr : GAP_LINK_ESTABLISHED_EVENT
  Gapbondmgr -> BLEStack : GAPBondMgr_LinkEst()
  Gapbondmgr -> BLEStack : GAP_Authenticate
  BLEStack -->] : Pairing req
  Gapbondmgr -> Application : Pairing state callback
  rnote over Application
  GAPBOND_PAIRING_
  STATE_STARTED
  end note

  == This section will vary depending on the pairing type.\nSee above examples for more information. ==

  BLEStack -->] : Encryption req
  BLEStack <--] : Encryption rsp
  BLEStack -> Gapbondmgr : GAP_AUTHENTICATION_\nCOMPLETE_EVENT

  rnote over Gapbondmgr
  Save bond info in NV
  end note

  Gapbondmgr -> Application : Pairing state callback
  rnote over Application
  GAPBOND_PAIRING_
  STATE_COMPLETE
  end note

  rnote over Application
  GAPBOND_PAIRING_
  STATE_BOND_SAVED
  end note

  == Eventually the connection may be terminated and re-established. ==

  BLEStack -> Gapbondmgr : GAP_LINK_ESTABLISHED_EVENT
  Gapbondmgr -> BLEStack : GAPBondMgr_LinkEst()

  rnote over Gapbondmgr
  Read bond info from NV.
  end note

  Gapbondmgr -> BLEStack : GAP_Bond()
  BLEStack -->] : Encryption req
  BLEStack <--] : Encryption rsp
  BLEStack -> Gapbondmgr : GAP_BOND_COMPLETE_\nEVENT
  Gapbondmgr -> Application : Pairing state callback
  rnote over Application
  GAPBOND_PAIRING_
  STATE_BONDED
  end note


@enduml

Figure 88. GAPBondMgr Example With Bonding Enabled.

Extract Bonding Information

After bonding, the local device can extract the bonding information saved in NV using gapBondMgrReadBondRec(). To successfully extract the bonding information, application will need to input the peer device’s address type and the peer device’s address. Those information are provided from the BLE5-Stack to the application when the link is established.

Following are the code snippet to extract the aforementioned parameters.

Listing 92. app_peripheral.c:: BLEAPPUTIL_LINK_ESTABLISHED_EVENT Extract peer device address and address type.
 1// LOCAL VARIABLES
 2
 3// Array to save peer device's address
 4static uint8_t peerDeviceAddr[B_ADDR_LEN];
 5
 6// enum to store peer device's address type
 7static GAP_Peer_Addr_Types_t pPeerAddrType;
 8
 9void Peripheral_GAPConnEventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
10{
11    switch(event)
12    {
13        case BLEAPPUTIL_LINK_ESTABLISHED_EVENT:
14        {
15            gapEstLinkReqEvent_t *gapEstMsg = (gapEstLinkReqEvent_t *)pMsgData;
16
17            if(gapEstMsg->connRole == BLEAPPUTIL_PERIPHERAL_ROLE)
18            {
19              //...
20              //...
21              if (gapEstMsg->hdr.status == SUCCESS)
22              {
23                  // Copy Peer's addr
24                  memcpy(peerDeviceAddr, gapEstMsg->devAddr, B_ADDR_LEN);
25
26                  // Copy Peer's addrType
27                  pPeerAddrType = (GAP_Peer_Addr_Types_t)(gapEstMsg->devAddrType & MASK_ADDRTYPE_ID);
28              }
29            //...
30            //...
31            }
32        }
33        break;
34      //...
35      //...

Once extracted the needed parameters, we can call gapBondMgrReadBondRec() by using the following code snippet.

Listing 93. Extract bonding information
 1// Parameters needed for storing bonding information.
 2static gapBondRec_t pSavedBondRec;
 3static gapBondLTK_t pLocalLtk;
 4static gapBondLTK_t pPeerLtk;
 5static uint8_t pPeerIRK[KEYLEN];
 6static uint8_t pPeerSRK[KEYLEN];
 7static uint32_t pPeerSignCount;
 8static gapBondCharCfg_t charCfg;
 9
10uint8_t readStatus = FAILURE;
11readStatus = gapBondMgrReadBondRec(pPeerAddrType,
12                                    peerDeviceAddr,
13                                    &pSavedBondRec,
14                                    &pLocalLtk,
15                                    &pPeerLtk,
16                                    pPeerIRK,
17                                    pPeerSRK,
18                                    pPeerSignCount,
19                                    &charCfg);
20if (readStatus == SUCCESS)
21{
22    // If read success, then export the data
23    // Here we will print it out for later use.
24    // For the print, we added the following defines
25    // Please consider your own example and modify as needed
26    Display_printf(dispHandle, dispIndex, 0, "#%5d    Peer Device Addr = [0x%02x, 0x%02x, 0x%02x, 0x%02x, 0x%02x, 0x%02x];", dispIndex,
27                    pSavedBondRec.addr[0],
28                    pSavedBondRec.addr[1],
29                    pSavedBondRec.addr[2],
30                    pSavedBondRec.addr[3],
31                    pSavedBondRec.addr[4],
32                    pSavedBondRec.addr[5]); dispIndex++;
33
34    Display_printf(dispHandle, dispIndex, 0, "#%5d    Peer Device AddrType = 0x%02x; stateFlag = 0x%02x;", dispIndex, pSavedBondRec.addrType, pSavedBondRec.stateFlags); dispIndex++;
35    Display_printf(dispHandle, dispIndex, 0, "#%5d    Peer Device AddrType = 0x%02x; stateFlag = 0x%02x;", dispIndex, pSavedBondRec.addrType, pSavedBondRec.stateFlags); dispIndex++;
36    Display_printf(dispHandle, dispIndex, 0, "#%5d    Local Device eDiv = 0x%02x; keySize = 0x%02x;", dispIndex, pLocalLtk.div, pLocalLtk.keySize); dispIndex++;
37    Display_printf(dispHandle, dispIndex, 0, "#%5d    Peer Device SignCount = 0x%08x;", dispIndex, pPeerSignCount); dispIndex++;
38    uint8 i;
39    for (i = 0; i < KEYLEN; i++)
40    {
41      Display_printf(dispHandle, dispIndex, 0, "#%5d    Local Device LTK[%d]= 0x%02x;", dispIndex, i, pLocalLtk.LTK[i]); dispIndex++;
42    }
43    for (i = 0; i < KEYLEN; i++)
44    {
45      Display_printf(dispHandle, dispIndex, 0, "#%5d    Peer Device IRK[%d]= 0x%02x;", dispIndex, i, pPeerIRK[i]); dispIndex++;
46    }
47    for (i = 0; i < KEYLEN; i++)
48    {
49      Display_printf(dispHandle, dispIndex, 0, "#%5d    Peer Device SRK[%d]= 0x%02x;", dispIndex, i, pPeerSRK[i]); dispIndex++;
50    }
51    for (i = 0; i < B_RANDOM_NUM_SIZE; i++)
52    {
53        Display_printf(dispHandle, dispIndex, 0, "#%5d    Local Device rand[%d]= 0x%02x;", dispIndex, i, pLocalLtk.rand[i]); dispIndex++;
54    }
55
56    Display_printf(dispHandle, dispIndex, 0, "#%5d    Charcfg attrHandle = 0x%04x; value = 0x%02x", dispIndex, charCfg.attrHandle, charCfg.value); dispIndex++;
57}
58break;

Warning

The pPeerLtk struct is not needed when extracting and importing bonds to another device. Therefore, we are not printing it out as the content of pPeerLtk is 0.

Import Bonding Information

The bond import feature is useful when for example, there are multiple Bluetooth LE devices as peripheral and one mobile phone as central, and you would like the phone to go through the pairing process only once but is able to establish an encrypted link with any other peripheral nodes.

The following content illustrates such usecase.

Note

Here we assume device A and device B have the same secondary address. The device address can be configured by either using HCI_EXT_SetBDADDRCmd() or through SysConfig tool –> Device Configuration –> Configure BLE Address.

After extracting bonding information from device A and transfer the information to device B, we can then add those information into NV for device B by using gapBondMgrImportBond().

Listing 94. App_StackInitDoneHandler Import bonding information
 1// Make sure the device B has the same BD address as device A
 2// For example, if the device A's address is the following
 3// Then use HCI_EXT_SetBDADDRCmd to change the device B's address
 4uint8_t bondImportTestAddr[B_ADDR_LEN] = {0x12, 0x34, 0x45, 0xFE, 0xCA, 0x98};
 5// Change device's address
 6HCI_EXT_SetBDADDRCmd(bondImportTestAddr);
 7
 8// Import Bond here
 9// Hardcode the bonding information from the printout
10pSavedBondRec.addr[0] = 0xf5;
11pSavedBondRec.addr[1] = 0xda;
12pSavedBondRec.addr[2] = 0x31;
13pSavedBondRec.addr[3] = 0xb0;
14pSavedBondRec.addr[4] = 0x6f;
15pSavedBondRec.addr[5] = 0x80;
16
17pSavedBondRec.addrType = PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID;
18pSavedBondRec.stateFlags = 0x1c;
19
20pLocalLtk.LTK[0]= 0xa8;
21pLocalLtk.LTK[1]= 0x82;
22pLocalLtk.LTK[2]= 0x09;
23pLocalLtk.LTK[3]= 0x19;
24pLocalLtk.LTK[4]= 0x65;
25pLocalLtk.LTK[5]= 0x01;
26pLocalLtk.LTK[6]= 0xbc;
27pLocalLtk.LTK[7]= 0x58;
28pLocalLtk.LTK[8]= 0x49;
29pLocalLtk.LTK[9]= 0x28;
30pLocalLtk.LTK[10]= 0x31;
31pLocalLtk.LTK[11]= 0xac;
32pLocalLtk.LTK[12]= 0x6c;
33pLocalLtk.LTK[13]= 0x50;
34pLocalLtk.LTK[14]= 0x6f;
35pLocalLtk.LTK[15]= 0xd2;
36
37pLocalLtk.div = 0;
38pLocalLtk.keySize = 0x10;
39
40pPeerLtk.div = 0;
41pPeerLtk.keySize = 0;
42uint8_t i;
43for (i = 0; i < B_RANDOM_NUM_SIZE; i++)
44{
45    pLocalLtk.rand[i] = 0;
46    pPeerLtk.rand[i] = 0;
47}
48
49for (i = 0; i < KEYLEN; i++)
50{
51    pPeerIRK[i] = 0;
52    pPeerLtk.LTK[i] = 0;
53}
54
55pPeerSRK[0]= 0xab;
56pPeerSRK[1]= 0x31;
57pPeerSRK[2]= 0x78;
58pPeerSRK[3]= 0xe5;
59pPeerSRK[4]= 0x5a;
60pPeerSRK[5]= 0x33;
61pPeerSRK[6]= 0xf6;
62pPeerSRK[7]= 0xe9;
63pPeerSRK[8]= 0x1b;
64pPeerSRK[9]= 0x80;
65pPeerSRK[10]= 0xeb;
66pPeerSRK[11]= 0xae;
67pPeerSRK[12]= 0x25;
68pPeerSRK[13]= 0xd4;
69pPeerSRK[14]= 0x1d;
70pPeerSRK[15]= 0x19;
71
72pPeerSignCount = 0;
73charCfg.attrHandle = 0xffff;
74charCfg.value = 0xff;
75
76gapBondMgrImportBond(&pSavedBondRec,
77                    &pLocalLtk,
78                    &pPeerLtk,
79                    pPeerIRK,
80                    pPeerSRK,
81                    pPeerSignCount,
82                    &charCfg);

The bonding import can be called at anytime, but for the demo purpose, we added the code under application_init. Therefore when device B connects with the central device that has paired with device A, the link between device B and central will be encrypted without going through the pairing process again.

Figure 89. illustrates the whole process of enable bonding, extract bonding information and import bonding information.

@startuml

  participant perA as "Peripheral A"
  participant cen as "Central"
  participant perB as "Peripheral B"

  cen --> perA : GAP_LINK_ESTABLISHED_EVENT
  cen --> perA : Pairing Req
  perA --> cen : Pairing Rsp

  == Depending on the combination of pairing req and pairing rsp, a type of pairing\nwill be selected. See above examples for more information. ==

  cen -> cen : Pairing state callback
  rnote over cen
    GAPBOND_PAIRING_
    STATE_STARTED
  end note

  perA -> perA : Pairing state callback
  rnote over perA
    GAPBOND_PAIRING_
    STATE_STARTED
  end note

  cen --> perA : Encryption req
  perA --> cen : Encryption rsp

  ...
  ... Both central and peripheral A will save the bond info in NV ...
  ...


  rnote over cen
    GAPBOND_PAIRING_
    STATE_COMPLETE
  end note

  rnote over perA
    GAPBOND_PAIRING_
    STATE_COMPLETE
  end note

  rnote over cen
    GAPBOND_PAIRING_
    STATE_BOND_SAVED
  end note

  rnote over perA
    GAPBOND_PAIRING_
    STATE_BOND_SAVED
  end note

  perA -> perA : Extract bonding information\nusing gapBondMgrReadBondRec

  ...
  ... Central can now terminate the link with Peripheral A ...
  ...

  perA -> perB : Transfer the bonding information through other wired/wireless protocols.\nFor example: LIN, CAN or SPI...etc

  perB -> perB : Save the bonding information to NV \nby using gapBondMgrImportBond
  cen --> perB : GAP_LINK_ESTABLISHED_EVENT

  cen --> perB : Encryption req
  perB --> cen : Encryption rsp

  ...
  ... Now the central and Peripheral B has an encrypted link \nwithout going through pairing process ...
  ...

@enduml

Figure 89. GAPBondMgr Example With Extracting and Importing Bonding Information.

GAPBondMgr and NV

The following components comprise one bonding entry:

1. Bond Record: this consists of the peer’s address, address type, privacy reconnection address, and state flags. This comprises 8 bytes and is defined as such:

// Structure of NV data for the connected device's address information
typedef struct
{
  /**
  * Peer's address
  *
  * If identity information exists for this bond, this will be an
  * identity address
  */
  uint8_t               addr[B_ADDR_LEN];
  /**
  * Peer's address type
  */
  GAP_Peer_Addr_Types_t addrType;
  /**
  * State flags of bond
  *
  * @ref GAP_BONDED_STATE_FLAGS
  */
  uint8_t               stateFlags;
} gapBondRec_t;

2. Client Characteristic Configurations (CCC): the amount of CCCs stored in each entry are set by the GAP_CHAR_CFG_MAX define. This is set to 4 by default. Each CCC is comprised of 4-bytes and is defined as follows:

// Structure of NV data for the connected device's characteristic configuration
typedef struct
{
  uint16 attrHandle;  // attribute handle
  uint8  value;       // attribute value for this device
} gapBondCharCfg_t;

3. Local Long Term Key (LTK) info: this stores the local device’s encryption information. This comprises 28 bytes and is composed as such:

typedef struct
{
  uint8   LTK[KEYLEN];              // Long Term Key (LTK)
  uint16  div;  //lint -e754        // LTK eDiv
  uint8   rand[B_RANDOM_NUM_SIZE];  // LTK random number
  uint8   keySize;                  // LTK key size
} gapBondLTK_t;

4. Peer Device Long Term Key Info: this stores the peer device’s encryption information. This is also a gapBondLTK_t and comprises 28 bytes.

5. Peer Device Identity Resolving Key (IRK): this stores the IRK generated during pairing. This is a 16-byte array.

6. Peer Device Connection Signature Resolving Key (CSRK): this stores the CSRK generated during pairing. This is a 16-byte array.

7. Peer Device Sign counter: this stores the sign counter generated during pairing. This is a 4-byte word.