SimpleLink Low Power F3 Core SDK 7.20.01.02 Release Notes
Table of Contents
Introduction
This is a GA release of the Core SDK 7.20.01.02 for Low Power F3 devices.
Documentation
Open the Documentation Overview file in the docs/ folder for a full list of documentation.
What’s New
- A summary of changes made in the current release of this product can be found in the product Change Log.
Host Support
See the SDK release notes for a description of which host operating systems are supported in this release.
Dependencies
See the SDK release notes for a description of which components and tools are required to work with this product.
Device Support
See the SDK release notes for a list of TI devices that are supported in this product.
Validation Information
The Core SDK was validated with the following components:
- Code Composer Studio 12.3.0
- GNU Code Generation Tools
- ARM GCC 9.2019.q4.major-0
- IAR Code Generation Tools
- ARM 9.32.1
- TI Clang Code Generation Tools
- ARM ti-cgt-armllvm_2.1.3.LTS-0
- FreeRTOS 202104.00-0
- SysConfig 1.10.0
- XDCTools 3.62.01.15
- Python 3.8.10
New Features
ID | Summary |
---|---|
TIDRIVERS-6110 | Add API for modular reduction for non-curve length input length |
TIDRIVERS-6025 | Add Elliptic Curve Integrated Encryption Scheme (ECIES) driver for CC23x0 |
Fixed Issues
ID | Summary |
---|---|
TIDRIVERS-6065 | Some PWM files not exported into SDK |
Known Issues
ID | Summary |
---|---|
None | None |
ID | Summary |
---|---|
TIPOSIX-4 | clock_nanosleep() with CLOCK_REALTIME broken on msp432 |
FREERTOS-8 | Tasks view in ROV for FreeRTOS does not show if a task is blocked on a semaphore or mutex |
Customer Support
- Use the E2E support forums for customer support.
- Use the External Bug and Enhancement System to track issues.
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
Prior Release Changes
A summary of changes made in previous releases of this product can be found in the product Change Log.