Data Fields
TaskP_Struct Union Reference

TaskP structure. More...

#include <TaskP.h>

Data Fields

uint32_t dummy
 
uint8_t data [(340)]
 

Detailed Description

TaskP structure.

Opaque structure that should be large enough to hold any of the RTOS specific TaskP objects.

Field Documentation

§ dummy

uint32_t TaskP_Struct::dummy

Align object

§ data

uint8_t TaskP_Struct::data[(340)]

The documentation for this union was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale