Structure for MCAN High Priority Message. More...
#include <MCAN.h>
Data Fields | |
uint32_t | bufIdx |
uint32_t | msi |
uint32_t | filterIdx |
uint32_t | filterList |
Structure for MCAN High Priority Message.
uint32_t MCAN_HighPriorityMsgInfo::bufIdx |
Buffer Index Only valid when MSI[1] = 1.
uint32_t MCAN_HighPriorityMsgInfo::msi |
Message Storage Indicator 0 = No FIFO selected 1 = FIFO message lost 2 = Message stored in FIFO 0 3 = Message stored in FIFO 1
uint32_t MCAN_HighPriorityMsgInfo::filterIdx |
Filter Index
uint32_t MCAN_HighPriorityMsgInfo::filterList |
Indicates the filter list of the matching filter element 0 = Standard Filter List 1 = Extended Filter List