TI BLE5-Stack API Documentation  3.02.02.00
Data Fields
l2capSignalEvent_t Struct Reference

OSAL L2CAP_SIGNAL_EVENT message format. More...

Data Fields

l2capSignalCmd_t cmd
 command data
 
uint16 connHandle
 connection message was received on
 
osal_event_hdr_t hdr
 L2CAP_SIGNAL_EVENT and status.
 
uint8 id
 identifier to match responses with requests
 
uint8 opcode
 type of command: L2CAP Signaling Codes (type of commands)
 

Detailed Description

OSAL L2CAP_SIGNAL_EVENT message format.

This message is used to deliver an incoming Signaling command up to an upper layer application.


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale