TI BLE5-Stack API Documentation  3.02.02.00
Enumerations
GapAdv Params

Enumerations

enum  GapAdv_ParamId_t {
  GAP_ADV_PARAM_PROPS, GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN, GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX, GAP_ADV_PARAM_PRIMARY_CHANNEL_MAP,
  GAP_ADV_PARAM_PEER_ADDRESS_TYPE, GAP_ADV_PARAM_PEER_ADDRESS, GAP_ADV_PARAM_FILTER_POLICY, GAP_ADV_PARAM_TX_POWER,
  GAP_ADV_PARAM_PRIMARY_PHY, GAP_ADV_PARAM_SECONDARY_PHY, GAP_ADV_PARAM_SID
}
 

Detailed Description

Params used in the GapAdv module

Enumeration Type Documentation

§ GapAdv_ParamId_t

GAP Advertising Parameters

These can be set with GapAdv_setParam and read with GapAdv_getParam. They do not have default values since it is required to pass a set of parameters into GapAdv_create

Each advertising handle can have a different set of parameters.

All parameters are readable and writable

Enumerator
GAP_ADV_PARAM_PROPS 

Advertising Event Properties

size: uint16_t

range: GapAdv_eventProps_t

GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN 

Minimum advertising interval (n * 0.625 ms)

This is for undirected and low duty cycle directed advertising

size: uint32_t

range: 20 ms to 10,485.759375 s

GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX 

Maximum advertising interval (n * 0.625 ms

This is for undirected and low duty cycle directed advertising

Note
This will be ignored as the GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN is always used

size: uint32_t

range: 20 ms to 10,485.759375 s

GAP_ADV_PARAM_PRIMARY_CHANNEL_MAP 

Primary Channel Map

A bit field that indicates the advertising channels that shall be used when transmitting advertising packets

size: uint8_t

range: GapAdv_advChannels_t

GAP_ADV_PARAM_PEER_ADDRESS_TYPE 

Peer Address Type for Directed Advertising

size: uint8_t

range: GAP_Peer_Addr_Types_t

GAP_ADV_PARAM_PEER_ADDRESS 

Peer Address for Directed Advertising

size: uint8_t[6]

range: 0x000000000000 - 0xFFFFFFFFFFFE

GAP_ADV_PARAM_FILTER_POLICY 

Advertising Filter Policy

size: uint8_t

range: GapAdv_filterPolicy_t

GAP_ADV_PARAM_TX_POWER 

Advertising Tx Power

This is the maximum power level at which the advertising packets are to be transmitted on the advertising channels. The Controller will choose a power level lower than or equal to this.

Note
When setting this parameter, the host will overwrite the value with the new chosen value if it is set successfully.
Warning
In order to set this parameter, GAP_ADV_PARAM_PROPS must be set to include GAP_ADV_PROP_TX_POWER

size: int8_t

units: dBm

range: -127 to +20 or GAP_ADV_TX_POWER_NO_PREFERENCE

GAP_ADV_PARAM_PRIMARY_PHY 

Primary PHY

The PHY on which the advertising packets are transmitted on the primary advertising channel.

size: uint8_t

range: GapAdv_primaryPHY_t

GAP_ADV_PARAM_SECONDARY_PHY 

Secondary PHY

The PHY on which the advertising packets are be transmitted on the secondary advertising channel.

size: uint8_t

range: GapAdv_secondaryPHY_t

GAP_ADV_PARAM_SID 

Advertising SID (set identity)

This is the value to be transmitted in the Advertising SID subfield of the ADI field of the Extended Header of those advertising channel PDUs that have an ADI field. If the advertising set only uses PDUs that do not contain an ADI field, this parameter is ignored.

size: uint8_t

range: 0-15

© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale