RCL Release Notes
Table of Contents
Introduction
The Radio Control Layer (RCL) component for the LPF3 SDK consists of:
- High-level Radio Control Layer driver providing scheduling and power management
- Low-level RF protocol implementation
- Radio core firmware images
- RF configuration arrays and settings
- API documentation
Disaclaimer
Future versions will have a change in the command status codes. See Upgrade and Compatibility Information for details.
Documentation
The following documentation is included in RCL.
- API documentation
- Release Notes (this document)
Build Size
The following is the output of the TI ARM Clang size tool:
| Component | Flash Size (Bytes) | RAM Size (Bytes) |
|---|---|---|
| LRF BLE Binaries | 8716 | 0 |
| LRF Generic PHY Binaries | 8396 | 0 |
| HAL | 964 | 102 |
| LRF | 3936 | 36 |
| RCL | 4452 | 0 |
| BLE5 Command Handler | 8447 | 0 |
| Generic PHY Command Handler | 6174 | 0 |
| ADC Noise Command Handler | 1212 | 0 |
| Totals | 42297 (8.07%) | 138 (0.37%) |
Note this is the total size of the archive, not necessarily the size of the final linked program.
Dependencies
- coresdk_lpf3: 7.20.00.03
- FreeRTOS: 202104.00-0
- TI ARM LLVM: 2.1.3.LTS-0
- GCC: 9.2019.q4.major-0
- IAR: 9.40.1-1
Hardware Setup
This release is tested with the following hardware:
- LP_EM_CC2340R5
No hardware modifications are required.
What’s New
This list contains all new features since: v7.20.00
| ID | Summary |
|---|---|
| RCL-409 | Improve robustness of radio entropy generation in the presence of a strong RF signal |
| RCL-238 | Added support for HFXT SW TCXO by compensating RF PLL |
Fixed Issues
This list contains all bugfixes since: v7.20.00
| ID | Summary |
|---|---|
| RCL-384 | RSSI read back-to-back reading sometimes returns unexpected value |
| RCL-392 | PBE fails to respond if a timer interrupt flag is unexpectedly set at first execution |
Known Issues
| ID | Summary |
|---|---|
| RCL-343 | PBE NESB - Address mismatch counter not implemented |
Upgrade and Compatibility Information
Future versions (7.30 and later) will provide more detailed information in the status field of an RCL command that has been stopped. This means that the identifiers of the RCL_CommandStatus enum will change. The values will also change; named identifiers should always be used when addressing variables of type RCL_CommandStatus.
| Identifier in this RCL version | Identifier in RCL version 7.30 and later | Description |
|---|---|---|
RCL_CommandStatus_Descheduled |
RCL_CommandStatus_DescheduledApi |
Command was descheduled before starting running in the radio because RCL_CommandStop() was called |
RCL_CommandStatus_Descheduled |
RCL_CommandStatus_DescheduledScheduling |
Command was descheduled before starting running in the radio due to scheduling of another command |
RCL_CommandStatus_GracefulStop |
RCL_CommandStatus_GracefulStopTimeout |
Command ended because time set in timing.relGracefulStopTime was reached |
RCL_CommandStatus_GracefulStop |
RCL_CommandStatus_GracefulStopApi |
Command ended gracefully because RCL_CommandStop() was called with RCL_StopType_Graceful argument |
RCL_CommandStatus_GracefulStop |
RCL_CommandStatus_GracefulStopScheduling |
Command ended due to scheduling where interrupting command had RCL_ConflictPolicy_Polite |
RCL_CommandStatus_HardStop |
RCL_CommandStatus_HardStopTimeout |
Command ended because time set in timing.relHardStopTime was reached |
RCL_CommandStatus_HardStop |
RCL_CommandStatus_HardStopApi |
Command ended because RCL_CommandStop() was called with RCL_StopType_Hard argument |
RCL_CommandStatus_HardStop |
RCL_CommandStatus_HardStopScheduling |
Command ended due to scheduling where interrupting command had RCL_ConflictPolicy_AlwaysInterrupt |
Code that checks for one of the statuses listed above for this version, should in the future check for any of the corresponding new statuses. The macros RCL_CommandStatus_isAnyDescheduled(), RCL_CommandStatus_isAnyGracefulStop(), and RCL_CommandStatus_isAnyHardStop() may be used for that purpose; these macros will give the same behavior both in this version and future versions.
Known Limitations
The following scenarios have limited test coverage in the RCL module tests:
- Stress testing or throughput testing of connection
- Testing of adding buffers to the radio while it is running
- The testing of fields in the
statsstructures - RF settings are provided statically as part of the RCL package. Eventually they will be provided as part of sysconfig.
The SW has the following limitations:
- Does not support Bluetooth 5 advertising extensions
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.