![]() |
![]() |
Task module for the RTOS Porting Interface.
============================================================================
TaskP objects are RTOS threads backed by OS-specific thread or task objects. Task functions will run according to the rules of the underlying scheduler, with higher priority tasks executing first.
Tasks require a stack and a control struct to operate, which can either be allocated statically with TaskP_construct or dynamically with TaskP_create. The stack should be large enough to contain at least your deepest call stack plus an interrupt frame.
Task Functions: The void* argument will be NULL by default, but you can set a value using TaskP_Params. Task functions should never return, as the behaviour after a task has returned is implementation-dependent and TaskP does not provide a mechanism for OS-independent task deletion. See your OS documentation for
#include <stdint.h>
#include <stdbool.h>
#include <stddef.h>
Go to the source code of this file.
Data Structures | |
union | TaskP_Struct |
TaskP structure. More... | |
struct | TaskP_Params |
Macros | |
#define | TaskP_STRUCT_SIZE (340) |
Number of bytes greater than or equal to the size of any RTOS Task object. More... | |
#define | TaskP_DEFAULT_STACK_SIZE (512) |
Number of bytes for the default stack size of any RTOS Task object. More... | |
Typedefs | |
typedef union TaskP_Struct | TaskP_Struct |
TaskP structure. More... | |
typedef TaskP_Struct * | TaskP_Handle |
Opaque client reference to an instance of a TaskP. More... | |
typedef void(* | TaskP_Function) (void *) |
Task function definition, passed to create and construct. More... | |
Enumerations | |
enum | TaskP_State { TaskP_State_RUNNING, TaskP_State_READY, TaskP_State_BLOCKED, TaskP_State_DELETED, TaskP_State_INACTIVE, TaskP_State_INVALID } |
Enum returned from TaskP_getState(). More... | |
Functions | |
TaskP_Handle | TaskP_create (TaskP_Function fxn, const TaskP_Params *params) |
Create a TaskP, allocating memory on the heap. More... | |
void | TaskP_delete (TaskP_Handle task) |
Delete a TaskP. More... | |
TaskP_Handle | TaskP_construct (TaskP_Struct *obj, TaskP_Function fxn, const TaskP_Params *params) |
Construct a TaskP from statically allocated memory. More... | |
void | TaskP_destruct (TaskP_Struct *obj) |
Destruct a TaskP. More... | |
TaskP_State | TaskP_getState (TaskP_Handle task) |
Get the current state of a task handle. More... | |
TaskP_Handle | TaskP_getCurrentTask (void) |
Get the currently executing task handle. More... | |
uintptr_t | TaskP_disableScheduler (void) |
Function to disable task scheduling. More... | |
void | TaskP_restoreScheduler (uintptr_t key) |
Function to re-enable task scheduling. More... | |
void | TaskP_yield (void) |
Create a scheduler point, yielding to equal priority tasks. More... | |
void | TaskP_Params_init (TaskP_Params *params) |
Initialize params structure to default values. More... | |
#define TaskP_STRUCT_SIZE (340) |
Number of bytes greater than or equal to the size of any RTOS Task object.
BIOS 6.x: 80 BIOS 7.x: 88 FreeRTOS: 104(llvm)/340(gcc)
#define TaskP_DEFAULT_STACK_SIZE (512) |
Number of bytes for the default stack size of any RTOS Task object.
typedef union TaskP_Struct TaskP_Struct |
TaskP structure.
Opaque structure that should be large enough to hold any of the RTOS specific TaskP objects.
typedef TaskP_Struct* TaskP_Handle |
Opaque client reference to an instance of a TaskP.
A TaskP_Handle returned from create or construct represents that instance.
typedef void(* TaskP_Function) (void *) |
Task function definition, passed to create and construct.
This function should never return.
enum TaskP_State |
Enum returned from TaskP_getState().
TaskP_Handle TaskP_create | ( | TaskP_Function | fxn, |
const TaskP_Params * | params | ||
) |
Create a TaskP, allocating memory on the heap.
Creates a new TaskP and registers it with the OS scheduler. The task object and the entire stack will be allocated on the heap - make sure you have a sufficiently large heap. Stack allocation size is controlled by params.
If the program is already executing a task and the new task has a higher priority the new task will be scheduled immediately; in this case TaskP_create() will not return until the new task blocks. To avoid this (for example when creating interdependent tasks at once) use TaskP_disableScheduler() and TaskP_restoreScheduler() to prevent the context switch.
TaskP | handle (NULL on failure) |
void TaskP_delete | ( | TaskP_Handle | task | ) |
Delete a TaskP.
Deletes a TaskP.
For FreeRTOS, INCLUDE_vTaskDelete has to be set to 1 in FreeRTOSConfig.h. See 'Configuration with FreeRTOS' in the Core SDK User's Guide for how to do this.
TaskP_Handle TaskP_construct | ( | TaskP_Struct * | obj, |
TaskP_Function | fxn, | ||
const TaskP_Params * | params | ||
) |
Construct a TaskP from statically allocated memory.
TaskP_construct creates a new task object. TaskP_construct returns the handle of the new task object or NULL if the task could not be created.
To use TaskP_construct you must set both point params.stack
to a valid preallocated memory location of at least params.stackSize
.
For FreeRTOS, configSUPPORT_STATIC_ALLOCATION has to be set to 1 in FreeRTOSConfig.h. See 'Configuration with FreeRTOS' in the Core SDK User's Guide for how to do this.
TaskP | handle (NULL on failure) |
void TaskP_destruct | ( | TaskP_Struct * | obj | ) |
Destruct a TaskP.
TaskP_destruct destructs a task object.
TaskP_State TaskP_getState | ( | TaskP_Handle | task | ) |
Get the current state of a task handle.
Returns the state of the referenced task at the time this function was called. The return value is not guaranteed to match the state of the task when the calling function tests the return value. For example, the referenced task might have unblocked as a result of an interrupt, but the value may still read TaskP_State_BLOCKED.
The conversion of task states between DPL, FreeRTOS and TI-RTOS is: DPL: FreeRTOS: TI-RTOS: TaskP_State_RUNNING - eRunning - Task_Mode_RUNNING TaskP_State_READY - eReady - Task_Mode_READY TaskP_State_BLOCKED - eBlocked - Task_Mode_BLOCKED TaskP_State_DELETED - eDeleted - Task_Mode_TERMINATED TaskP_State_INACTIVE - eSuspended - Task_Mode_INACTIVE TaskP_State_INVALID - eInvalid - N.A
For FreeRTOS, INCLUDE_eTaskGetState has to be set to 1 in FreeRTOSConfig.h. See 'Configuration with FreeRTOS' in the Core SDK User's Guide for how to do this.
Current | state of the task pointed to by the task parameter |
TaskP_Handle TaskP_getCurrentTask | ( | void | ) |
Get the currently executing task handle.
For FreeRTOS, INCLUDE_xTaskGetCurrentTaskHandle has to be set to 1 in FreeRTOSConfig.h. See 'Configuration with FreeRTOS' in the Core SDK User's Guide for how to do this.
The | handle for the calling task |
uintptr_t TaskP_disableScheduler | ( | void | ) |
Function to disable task scheduling.
This function can be called multiple times, but must unwound in the reverse order. For example
For FreeRTOS the key value returned is always 0.
void TaskP_restoreScheduler | ( | uintptr_t | key | ) |
Function to re-enable task scheduling.
For FreeRTOS the key value is ignored.
key | returned from TaskP_disableScheduler |
void TaskP_yield | ( | void | ) |
Create a scheduler point, yielding to equal priority tasks.
Task_yield yields the processor to another task of equal priority. A task switch occurs when you call Task_yield if there is an equal priority task ready to run.
void TaskP_Params_init | ( | TaskP_Params * | params | ) |
Initialize params structure to default values.
Initialize the parameter struct with default values.
params | pointer to the task parameter struct |