TI BLE5-Stack API Documentation  3.02.02.00
Modules | Files | Macros | Functions
LinkDB

Modules

 GapInit Constants
 
 

Files

file  linkdb.h
 

Macros

#define linkDB_Authenticated(connectionHandle)   linkDB_State( (connectionHandle), LINK_AUTHENTICATED )
 
#define linkDB_Bonded(connectionHandle)   linkDB_State( (connectionHandle), LINK_BOUND )
 
#define linkDB_Encrypted(connectionHandle)   linkDB_State( (connectionHandle), LINK_ENCRYPTED )
 
#define linkDB_Up(connectionHandle)   linkDB_State( (connectionHandle), LINK_CONNECTED )
 

Functions

uint8 linkDB_GetInfo (uint16 connectionHandle, linkDBInfo_t *pInfo)
 
uint8 linkDB_NumActive (void)
 
uint8 linkDB_NumConns (void)
 
uint8 linkDB_State (uint16 connectionHandle, uint8 state)
 

Detailed Description

This module implements the Link Database Module

Macro Definition Documentation

§ linkDB_Authenticated

#define linkDB_Authenticated (   connectionHandle)    linkDB_State( (connectionHandle), LINK_AUTHENTICATED )

Check to see if the physical link is authenticated.

Parameters
connectionHandlecontroller link connection handle.
Returns
TRUE if the link is authenticated
FALSE, otherwise.

§ linkDB_Bonded

#define linkDB_Bonded (   connectionHandle)    linkDB_State( (connectionHandle), LINK_BOUND )

Check to see if the physical link is bonded.

Parameters
connectionHandlecontroller link connection handle.
Returns
TRUE if the link is bonded
FALSE, otherwise.

§ linkDB_Encrypted

#define linkDB_Encrypted (   connectionHandle)    linkDB_State( (connectionHandle), LINK_ENCRYPTED )

Check to see if the physical link is encrypted.

Parameters
connectionHandlecontroller link connection handle.
Returns
TRUE if the link is encrypted
FALSE, otherwise.

§ linkDB_Up

#define linkDB_Up (   connectionHandle)    linkDB_State( (connectionHandle), LINK_CONNECTED )

Check to see if a physical link is up (connected).

Parameters
connectionHandlecontroller link connection handle.
Returns
TRUE if the link is up
FALSE, otherwise.

Function Documentation

§ linkDB_GetInfo()

uint8 linkDB_GetInfo ( uint16  connectionHandle,
linkDBInfo_t pInfo 
)

Get information about a link

Copies all of the link information into pInfo. Uses the connection handle to search the link database.

Parameters
connectionHandlecontroller link connection handle.
pInfooutput parameter to copy the link information
Returns
SUCCESS
FAILURE connection wasn't found

§ linkDB_NumActive()

uint8 linkDB_NumActive ( void  )

Return the number of active connections

Returns
the number of active connections

§ linkDB_NumConns()

uint8 linkDB_NumConns ( void  )

Return the maximum number of connections supported.

Returns
the number of connections supported

§ linkDB_State()

uint8 linkDB_State ( uint16  connectionHandle,
uint8  state 
)

Check to see if a physical link is in a specific state.

Parameters
connectionHandlecontroller link connection handle.
stateLinkDB Connection State Flags state to look for.
Returns
TRUE if the link is found and state is set in state flags.
FALSE otherwise.
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale