Data Fields
ECDSA_Params Struct Reference

ECDSA Parameters. More...

#include <ECDSA.h>

Collaboration diagram for ECDSA_Params:
Collaboration graph
[legend]

Data Fields

ECDSA_ReturnBehavior returnBehavior
 
ECDSA_CallbackFxn callbackFxn
 
uint32_t timeout
 
void * custom
 

Detailed Description

ECDSA Parameters.

ECDSA Parameters are used to with the ECDSA_open() call. Default values for these parameters are set using ECDSA_Params_init().

See also
ECDSA_Params_init()

Field Documentation

§ returnBehavior

ECDSA_ReturnBehavior ECDSA_Params::returnBehavior

Blocking, callback, or polling return behavior

§ callbackFxn

ECDSA_CallbackFxn ECDSA_Params::callbackFxn

Callback function pointer

§ timeout

uint32_t ECDSA_Params::timeout

Timeout in system ticks before the operation fails and returns

§ custom

void* ECDSA_Params::custom

Custom argument used by driver implementation


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale