![]() |
![]() |
ComparatorLPF3LP Object. More...
#include <ComparatorLPF3LP.h>
Data Fields | |
HwiP_Struct | hwi |
Comparator_CallBackFxn | callbackFxn |
Comparator_Trigger | trigger |
bool | isOpen |
bool | isRunning |
ComparatorLPF3LP Object.
The application must not access any member variables of this structure!
HwiP_Struct ComparatorLPF3LP_Object::hwi |
Hwi used for handling comparator events
Comparator_CallBackFxn ComparatorLPF3LP_Object::callbackFxn |
User callback function
Comparator_Trigger ComparatorLPF3LP_Object::trigger |
Condition on which comparator triggers an event
bool ComparatorLPF3LP_Object::isOpen |
Determine if comparator is open
bool ComparatorLPF3LP_Object::isRunning |
Determine if comparator instance is already running