![]() |
![]() |
AESCBCLPF3 Object. More...
#include <AESCBCLPF3.h>
Data Fields | |
AESCommonLPF3_Object | common |
volatile uint32_t | iv [AES_IV_LENGTH_BYTES/4] |
AESCBC_CallbackFxn | callbackFxn |
AESCBC_OperationUnion * | operation |
AESCBC_OperationType | operationType |
bool | threadSafe |
AESCBCLPF3 Object.
The application must not access any member variables of this structure!
AESCommonLPF3_Object AESCBCLPF3_Object::common |
volatile uint32_t AESCBCLPF3_Object::iv[AES_IV_LENGTH_BYTES/4] |
AESCBC_CallbackFxn AESCBCLPF3_Object::callbackFxn |
AESCBC_OperationUnion* AESCBCLPF3_Object::operation |
AESCBC_OperationType AESCBCLPF3_Object::operationType |
bool AESCBCLPF3_Object::threadSafe |