![]() |
![]() |
![]() |
Macros | |
#define | SPI_STATUS_SUCCESS (0) |
Successful status code returned by SPI_control(). More... | |
#define | SPI_STATUS_ERROR (-1) |
Generic error status code returned by SPI_control(). More... | |
#define | SPI_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by SPI_control() for undefined command codes. More... | |
SPI_STATUS_* macros are general status codes returned by SPI_control()
SPILPF3DMA_STATUS_* macros are command codes only defined in the SPILPF3DMA.h driver implementation and need to:
#define SPI_STATUS_SUCCESS (0) |
Successful status code returned by SPI_control().
This value is returned from SPI_control() if the control code was executed successfully.
#define SPI_STATUS_ERROR (-1) |
Generic error status code returned by SPI_control().
This value is returned from SPI_control() if the control code was not executed successfully.
#define SPI_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by SPI_control() for undefined command codes.
This value is returned from SPI_control() if the control code is not recognized by the driver implementation.