|
| This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming | interface (API) which enables seamless migration across the SimpleLink SDK portfolio. Unless specifically stated otherwise |
| | [drivers_common_overview] More...
|
| |
| This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating | system (RTOS) application. All TI-Driver implementations utilize the Power driver APIs to ensure low power consumption at all times. The drivers support TI-RTOS7(SYS/BIOS) |
| |
| This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating and NoRTOS with examples provided for each variant the drivers are supported by SysConfig to enable easy re configuration of the drivers par and NoRTOS</b > li< b > Thread safe APIs</b > li< b > SysConfig support</b > li< b > Example usage</b > li< b > Power management support</b > par Driver Initialization parblock TI Driver APIs follow a common initialization model This model typically consists and close the driver Unless otherwise the initialization< b > may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open< b > it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref< b > Driver_config</b > Multiple software entities may use the same driver concurrently For a Bluetooth or WiFi stack may utilize a driver instance The application may concurrently use the same driver assuming it has opened a unique instance of the driver Let s examine the ADC driver for example include Driver_init h A couple observations from this code | ADC_init (). 4. We have to create a handle for our ADC driver instance. This is done by calling ADC_open() with our desired config index. Once a handle has been created the driver instance is ready for use. Each index can only be opened once! 4. In this simple example |
| | Function to initialize the ADC driver. More...
|
| |
| This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating and NoRTOS with examples provided for each variant the drivers are supported by SysConfig to enable easy re configuration of the drivers par and NoRTOS</b > li< b > Thread safe APIs</b > li< b > SysConfig support</b > li< b > Example usage</b > li< b > Power management support</b > par Driver Initialization parblock TI Driver APIs follow a common initialization model This model typically consists and close the driver Unless otherwise the initialization< b > may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open< b > it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref< b > Driver_config</b > Multiple software entities may use the same driver concurrently For a Bluetooth or WiFi stack may utilize a driver instance The application may concurrently use the same driver assuming it has opened a unique instance of the driver Let s examine the ADC driver for example include Driver_init h A couple observations from this code we use the | ADC_convert () API. 5. A driver instance can be closed and re-open. For our simple example |
| |
|
| This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating | FreeRTOS |
| |
| This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating and NoRTOS with examples provided for each variant | Lastly |
| |
| This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating and NoRTOS with examples provided for each variant the drivers are supported by SysConfig to enable easy re configuration of the drivers par | Features |
| |
| This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating and NoRTOS with examples provided for each variant the drivers are supported by SysConfig to enable easy re configuration of the drivers par and NoRTOS</b > li< b > Thread safe APIs</b > li< b > SysConfig support</b > li< b > Example usage</b > li< b > Power management support</b > par Driver Initialization parblock TI Driver APIs follow a common initialization model This model typically consists | of |
| |
| This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating and NoRTOS with examples provided for each variant the drivers are supported by SysConfig to enable easy re configuration of the drivers par and NoRTOS</b > li< b > Thread safe APIs</b > li< b > SysConfig support</b > li< b > Example usage</b > li< b > Power management support</b > par Driver Initialization parblock TI Driver APIs follow a common initialization model This model typically consists | open |
| |
| This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating and NoRTOS with examples provided for each variant the drivers are supported by SysConfig to enable easy re configuration of the drivers par and NoRTOS</b > li< b > Thread safe APIs</b > li< b > SysConfig support</b > li< b > Example usage</b > li< b > Power management support</b > par Driver Initialization parblock TI Driver APIs follow a common initialization model This model typically consists | use |
| |
| This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating and NoRTOS with examples provided for each variant the drivers are supported by SysConfig to enable easy re configuration of the drivers par and NoRTOS</b > li< b > Thread safe APIs</b > li< b > SysConfig support</b > li< b > Example usage</b > li< b > Power management support</b > par Driver Initialization parblock TI Driver APIs follow a common initialization model This model typically consists and close the driver Unless otherwise | stated |
| |
| This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating and NoRTOS with examples provided for each variant the drivers are supported by SysConfig to enable easy re configuration of the drivers par and NoRTOS</b > li< b > Thread safe APIs</b > li< b > SysConfig support</b > li< b > Example usage</b > li< b > Power management support</b > par Driver Initialization parblock TI Driver APIs follow a common initialization model This model typically consists and close the driver Unless otherwise the initialization | function |
| |
| This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating and NoRTOS with examples provided for each variant the drivers are supported by SysConfig to enable easy re configuration of the drivers par and NoRTOS</b > li< b > Thread safe APIs</b > li< b > SysConfig support</b > li< b > Example usage</b > li< b > Power management support</b > par Driver Initialization parblock TI Driver APIs follow a common initialization model This model typically consists and close the driver Unless otherwise the initialization< b > | Driver_init</b > |
| |
| This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating and NoRTOS with examples provided for each variant the drivers are supported by SysConfig to enable easy re configuration of the drivers par and NoRTOS</b > li< b > Thread safe APIs</b > li< b > SysConfig support</b > li< b > Example usage</b > li< b > Power management support</b > par Driver Initialization parblock TI Driver APIs follow a common initialization model This model typically consists and close the driver Unless otherwise the initialization< b > may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open< b > | Driver_open</b > |
| |
| This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating and NoRTOS with examples provided for each variant the drivers are supported by SysConfig to enable easy re configuration of the drivers par and NoRTOS</b > li< b > Thread safe APIs</b > li< b > SysConfig support</b > li< b > Example usage</b > li< b > Power management support</b > par Driver Initialization parblock TI Driver APIs follow a common initialization model This model typically consists and close the driver Unless otherwise the initialization< b > may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open< b > it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref | driver_configuration |
| |
| This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating and NoRTOS with examples provided for each variant the drivers are supported by SysConfig to enable easy re configuration of the drivers par and NoRTOS</b > li< b > Thread safe APIs</b > li< b > SysConfig support</b > li< b > Example usage</b > li< b > Power management support</b > par Driver Initialization parblock TI Driver APIs follow a common initialization model This model typically consists and close the driver Unless otherwise the initialization< b > may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open< b > it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref< b > Driver_config</b > Multiple software entities may use the same driver concurrently For | example |
| |
| This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating and NoRTOS with examples provided for each variant the drivers are supported by SysConfig to enable easy re configuration of the drivers par and NoRTOS</b > li< b > Thread safe APIs</b > li< b > SysConfig support</b > li< b > Example usage</b > li< b > Power management support</b > par Driver Initialization parblock TI Driver APIs follow a common initialization model This model typically consists and close the driver Unless otherwise the initialization< b > may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open< b > it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref< b > Driver_config</b > Multiple software entities may use the same driver concurrently For a Bluetooth or WiFi stack may utilize a driver instance The application may concurrently use the same driver assuming it has opened a unique instance of the driver Let s examine the ADC driver for example include Driver_init h A couple observations from this code we use the that s all we need | However |
| |
| This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating and NoRTOS with examples provided for each variant the drivers are supported by SysConfig to enable easy re configuration of the drivers par and NoRTOS</b > li< b > Thread safe APIs</b > li< b > SysConfig support</b > li< b > Example usage</b > li< b > Power management support</b > par Driver Initialization parblock TI Driver APIs follow a common initialization model This model typically consists and close the driver Unless otherwise the initialization< b > may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open< b > it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref< b > Driver_config</b > Multiple software entities may use the same driver concurrently For a Bluetooth or WiFi stack may utilize a driver instance The application may concurrently use the same driver assuming it has opened a unique instance of the driver Let s examine the ADC driver for example include Driver_init h A couple observations from this code we use the that s all we need for full details on the ADC and other | drivers |
| |
| This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating and NoRTOS with examples provided for each variant the drivers are supported by SysConfig to enable easy re configuration of the drivers par and NoRTOS</b > li< b > Thread safe APIs</b > li< b > SysConfig support</b > li< b > Example usage</b > li< b > Power management support</b > par Driver Initialization parblock TI Driver APIs follow a common initialization model This model typically consists and close the driver Unless otherwise the initialization< b > may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open< b > it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref< b > Driver_config</b > Multiple software entities may use the same driver concurrently For a Bluetooth or WiFi stack may utilize a driver instance The application may concurrently use the same driver assuming it has opened a unique instance of the driver Let s examine the ADC driver for example include Driver_init h A couple observations from this code we use the that s all we need for full details on the ADC and other reference the< b > Drivers and Documentation</b > section below endparblock *******************************************************************************The Display driver is designed abstract to operations &considerations specific to a given output method *******************************************************************************< TABLE >< TR align="center">< TH > Display Driver Interface</TH >< TH > Implementations</TH ></TR >< TR align="center">< TD > ref Display h</TD >< TD > ref DisplayHost h n ref DisplayUart2 h</TD ></TR ></TABLE > *******************************************************************************< TABLE >< TR align="center">< TH > Display Driver Interface</TH >< TH > Implementations</TH ></TR >< TR align="center">< TD > ref Display h</TD >< TD > ref DisplaySharp h n ref DisplayHost h n ref DisplayExt h n ref DisplayUart2 h</TD ></TR ></TABLE > *******************************************************************************Logging is a lightweight framework for instrumenting target code *******************************************************************************< TABLE >< TR align="center">< TH > Log Interface</TH >< TH > Sinks</TH ></TR >< TR align="center">< TD >< a class="el" href="../../../tiutils/html/group__ti__log__LOG.html"> Log h</a ></TD >< TD > ref LogSinkBuf h</TD ></TR ></TABLE > *******************************************************************************< TABLE >< TR align="center">< TH > Log Interface</TH >< TH > Sinks</TH ></TR >< TR align="center">< TD >< a class="el" href="../../../tiutils/html/group__ti__log__LOG.html"> Log h</a ></TD >< TD > ref LogSinkBuf h n ref LogSinkITM h</TD ></TR ></TABLE > *******************************************************************************The NoRTOS framework module is provided to enable use of drivers without an underlying operating system The module provides interfaces used by drivers to perform | delays |
| | [drivers_common_overview] More...
|
| |
| This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating and NoRTOS with examples provided for each variant the drivers are supported by SysConfig to enable easy re configuration of the drivers par and NoRTOS</b > li< b > Thread safe APIs</b > li< b > SysConfig support</b > li< b > Example usage</b > li< b > Power management support</b > par Driver Initialization parblock TI Driver APIs follow a common initialization model This model typically consists and close the driver Unless otherwise the initialization< b > may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open< b > it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref< b > Driver_config</b > Multiple software entities may use the same driver concurrently For a Bluetooth or WiFi stack may utilize a driver instance The application may concurrently use the same driver assuming it has opened a unique instance of the driver Let s examine the ADC driver for example include Driver_init h A couple observations from this code we use the that s all we need for full details on the ADC and other reference the< b > Drivers and Documentation</b > section below endparblock *******************************************************************************The Display driver is designed abstract to operations &considerations specific to a given output method *******************************************************************************< TABLE >< TR align="center">< TH > Display Driver Interface</TH >< TH > Implementations</TH ></TR >< TR align="center">< TD > ref Display h</TD >< TD > ref DisplayHost h n ref DisplayUart2 h</TD ></TR ></TABLE > *******************************************************************************< TABLE >< TR align="center">< TH > Display Driver Interface</TH >< TH > Implementations</TH ></TR >< TR align="center">< TD > ref Display h</TD >< TD > ref DisplaySharp h n ref DisplayHost h n ref DisplayExt h n ref DisplayUart2 h</TD ></TR ></TABLE > *******************************************************************************Logging is a lightweight framework for instrumenting target code *******************************************************************************< TABLE >< TR align="center">< TH > Log Interface</TH >< TH > Sinks</TH ></TR >< TR align="center">< TD >< a class="el" href="../../../tiutils/html/group__ti__log__LOG.html"> Log h</a ></TD >< TD > ref LogSinkBuf h</TD ></TR ></TABLE > *******************************************************************************< TABLE >< TR align="center">< TH > Log Interface</TH >< TH > Sinks</TH ></TR >< TR align="center">< TD >< a class="el" href="../../../tiutils/html/group__ti__log__LOG.html"> Log h</a ></TD >< TD > ref LogSinkBuf h n ref LogSinkITM h</TD ></TR ></TABLE > *******************************************************************************The NoRTOS framework module is provided to enable use of drivers without an underlying operating system The module provides interfaces used by drivers to perform block | execution |
| |