Data Structures | Enumerations | Variables
ADCLPF3.h File Reference

Detailed Description

ADC driver implementation for the ADC peripheral on Low Power F3 devices.


This ADC driver implementation is designed to operate on a ADC peripheral for Low Power F3 devices.

Refer to ADC.h for a complete description of APIs & example of use.

#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/ADC.h>
#include <ti/drivers/Power.h>
#include <ti/devices/DeviceFamily.h>
#include <DeviceFamily_constructPath(driverlib/adc.h)>
Include dependency graph for ADCLPF3.h:

Go to the source code of this file.

Data Structures

struct  ADCLPF3_HWAttrs
 ADCLPF3 Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. More...
 
struct  ADCLPF3_Object
 ADCLPF3 Object. More...
 

Enumerations

enum  ADCLPF3_Resolution_Bits { ADCLPF3_RESOLUTION_12_BIT = ADC_RESOLUTION_12_BIT, ADCLPF3_RESOLUTION_10_BIT = ADC_RESOLUTION_10_BIT, ADCLPF3_RESOLUTION_8_BIT = ADC_RESOLUTION_8_BIT }
 Resolution of ADC-conversion. More...
 
enum  ADCLPF3_Reference_Source { ADCLPF3_FIXED_REFERENCE_1V4 = ADC_FIXED_REFERENCE_1V4, ADCLPF3_FIXED_REFERENCE_2V5 = ADC_FIXED_REFERENCE_2V5, ADCLPF3_VDDS_REFERENCE = ADC_VDDS_REFERENCE, ADCLPF3_EXTERNAL_REFERENCE = ADC_EXTERNAL_REFERENCE }
 Specifies the source of the ADC reference voltage. More...
 
enum  ADCLPF3_Clock_Divider {
  ADCLPF3_CLKDIV_1 = ADC_CLOCK_DIVIDER_1, ADCLPF3_CLKDIV_2 = ADC_CLOCK_DIVIDER_2, ADCLPF3_CLKDIV_4 = ADC_CLOCK_DIVIDER_4, ADCLPF3_CLKDIV_8 = ADC_CLOCK_DIVIDER_8,
  ADCLPF3_CLKDIV_16 = ADC_CLOCK_DIVIDER_16, ADCLPF3_CLKDIV_24 = ADC_CLOCK_DIVIDER_24, ADCLPF3_CLKDIV_32 = ADC_CLOCK_DIVIDER_32, ADCLPF3_CLKDIV_48 = ADC_CLOCK_DIVIDER_48
}
 ADC clock-divider. More...
 

Variables

const ADC_FxnTable ADCLPF3_fxnTable
 

Enumeration Type Documentation

§ ADCLPF3_Resolution_Bits

Resolution of ADC-conversion.

This sets the resolution of the ADC conversion, and will affect how long a conversion takes.

Enumerator
ADCLPF3_RESOLUTION_12_BIT 
ADCLPF3_RESOLUTION_10_BIT 
ADCLPF3_RESOLUTION_8_BIT 

§ ADCLPF3_Reference_Source

Specifies the source of the ADC reference voltage.

  • The ADC reference voltage will determine the upper limit of the input voltage.
Note
The actual reference values are slightly different for each device and are higher than the values specified above. This gain is saved in the FCFG. The function ADC_convertToMicroVolts() must be used to derive actual voltage values. Do not attempt to compare raw values between devices or derive a voltage from them yourself. The results of doing so will only be approximately correct.
Warning
Refer to the datasheet to make sure the input voltage to the ADC never exceeds the specifies limits.
Enumerator
ADCLPF3_FIXED_REFERENCE_1V4 
ADCLPF3_FIXED_REFERENCE_2V5 
ADCLPF3_VDDS_REFERENCE 
ADCLPF3_EXTERNAL_REFERENCE 

§ ADCLPF3_Clock_Divider

ADC clock-divider.

This sets the clock divider value for the ADC clock, derived from the SYSCLK

Enumerator
ADCLPF3_CLKDIV_1 
ADCLPF3_CLKDIV_2 
ADCLPF3_CLKDIV_4 
ADCLPF3_CLKDIV_8 
ADCLPF3_CLKDIV_16 
ADCLPF3_CLKDIV_24 
ADCLPF3_CLKDIV_32 
ADCLPF3_CLKDIV_48 

Variable Documentation

§ ADCLPF3_fxnTable

const ADC_FxnTable ADCLPF3_fxnTable
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale