Instance: RTC
Component: RTC
Base address: 0x40002000
ULL Real Time Clock module
RTC includes 2 channels.
- Channel 0 is a compare channel
- Channel 1 is a capture channel
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
RO |
32 |
0x6442 1010 |
0x0000 0000 |
0x4000 2000 |
|
RW |
32 |
0x0000 0000 |
0x0000 0004 |
0x4000 2004 |
|
RW |
32 |
0x0000 0000 |
0x0000 0008 |
0x4000 2008 |
|
RW |
32 |
0x0000 0000 |
0x0000 000C |
0x4000 200C |
|
RO |
32 |
0x0000 0000 |
0x0000 0018 |
0x4000 2018 |
|
RO |
32 |
0x0000 0000 |
0x0000 001C |
0x4000 201C |
|
RW |
32 |
0x0000 0000 |
0x0000 0028 |
0x4000 2028 |
|
RO |
32 |
0x0000 0000 |
0x0000 0038 |
0x4000 2038 |
|
RW |
32 |
0x0000 0000 |
0x0000 003C |
0x4000 203C |
|
RW |
32 |
0x0000 0000 |
0x0000 0044 |
0x4000 2044 |
|
RO |
32 |
0x0000 0000 |
0x0000 0048 |
0x4000 2048 |
|
RO |
32 |
0x0000 0000 |
0x0000 004C |
0x4000 204C |
|
WO |
32 |
0x0000 0000 |
0x0000 0050 |
0x4000 2050 |
|
WO |
32 |
0x0000 0000 |
0x0000 0054 |
0x4000 2054 |
|
WO |
32 |
0x0000 0000 |
0x0000 0058 |
0x4000 2058 |
|
WO |
32 |
0x0000 0000 |
0x0000 005C |
0x4000 205C |
|
RW |
32 |
0x0000 0000 |
0x0000 0060 |
0x4000 2060 |
|
RW |
32 |
0x0000 0000 |
0x0000 0064 |
0x4000 2064 |
Address Offset | 0x0000 0000 | ||
Physical Address | 0x4000 2000 | Instance | 0x4000 2000 |
Description | Description Register. This register provides IP module ID, revision information, instance index and standard MMR registers offset. | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:16 | MODID | Module identifier used to uniquely identify this IP. | RW | 0x6442 | ||
15:12 | STDIPOFF | Standard IP MMR block offset. Standard IP MMRs are the set of from aggregated IRQ registers till DTB. 0: Standard IP MMRs do not exist 0x1-0xF: Standard IP MMRs begin at offset of (64*STDIPOFF from the base IP address) |
RW | 0x1 | ||
11:8 | INSTIDX | IP Instance ID number. If multiple instances of IP exist in the device, this field can identify the instance number (0-15). | RW | 0x0 | ||
7:4 | MAJREV | Major revision of IP (0-15). | RW | 0x1 | ||
3:0 | MINREV | Minor revision of IP (0-15). | RW | 0x0 |
Address Offset | 0x0000 0004 | ||
Physical Address | 0x4000 2004 | Instance | 0x4000 2004 |
Description | RTC Control register. This register controls resetting the of RTC counter | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
0 | RST | RTC counter reset. Writing 1 to this bit will reset the RTC counter, and cause it to resume counting from 0x0
|
WO | 0 |
Address Offset | 0x0000 0008 | ||
Physical Address | 0x4000 2008 | Instance | 0x4000 2008 |
Description | RTC channel mode set register. Read to each bit field of this register provides the current channel mode. - Read of 1'b0 indicates the channel is unarmed. - Read of 1'b1 indicates the channel is either in capture or compare mode. A write to each bitfield of this register the following effect: - Write of 1'b0 has no effect on channel mode. - Write of 1'b1 has no effect on the compare channel. While write of 1'b1 for capture channel will arm it in capture mode if it is disabled. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
1 | CH1 | Arming Channel 1 for capture operation.
|
RW | 0 | |||||||||||
0 | CH0 | No effect on arming the channel. Read will give the status of the Channel 0.
|
RW | 0 |
Address Offset | 0x0000 000C | ||
Physical Address | 0x4000 200C | Instance | 0x4000 200C |
Description | RTC channel mode clear register. Read to each bit field of this register provides the current channel mode. - Read of 1'b0 indicates the channel is unarmed. - Read of 1'b1 indicates the channel is either in capture or compare mode. A write to each bitfield of this register the following effect: - Write of 1'b0 has no effect on channel mode. - Write of 1'b1 for capture/compare channel will disarm it without triggering event unless a compare/capture event happens in the same cycle. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
1 | CH1 | Disarming Channel 1
|
RW | 0 | |||||||||||
0 | CH0 | Disarming Channel 0
|
RW | 0 |
Address Offset | 0x0000 0018 | ||
Physical Address | 0x4000 2018 | Instance | 0x4000 2018 |
Description | RTC Time value register. 32-bit unsigned integer representing [34:3] time slice of the real time clock counter. The counter runs on LFCLK. This field has a resolution of 8us, and range of about 9.5 hours. | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:0 | VAL | Unsigned integer representing [34:3]slice of real time counter. | RO | 0x0000 0000 |
Address Offset | 0x0000 001C | ||
Physical Address | 0x4000 201C | Instance | 0x4000 201C |
Description | RTC time value register. 32-bit unsigned integer representing [50:19] time slice of the real time clock counter. This field has a resolution of about 0.5s and a range of about 71.4 years. | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:0 | VAL | Unsigned integer representing. [50:19]slice of real time counter. | RO | 0x0000 0000 |
Address Offset | 0x0000 0028 | ||
Physical Address | 0x4000 2028 | Instance | 0x4000 2028 |
Description | Channel 0 compare value. A write to this register automatically enables the channel to trigger an event when RTC timer reaches the programmed value or if the programmed value is 1 sec in the past. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | VAL | RTC Channel 0 compare value. This value is compared against TIME8U.VAL. A Channel 0 event is generated when TIME8U.VAL value reaches or exceeds this compare value. | RW | 0x0000 0000 |
Address Offset | 0x0000 0038 | ||
Physical Address | 0x4000 2038 | Instance | 0x4000 2038 |
Description | Channel 1 capture value. This register captures the RTC time slice [34:3] on each selected edge of the capture event when the ARMSET.CH1 = 1. | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:21 | RESERVED21 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 | ||
20:0 | VAL | TIME8U.VAL captured value at the last selected edge of capture event. | RO | 0b0 0000 0000 0000 0000 0000 |
Address Offset | 0x0000 003C | ||
Physical Address | 0x4000 203C | Instance | 0x4000 203C |
Description | Channel 1 configuration register. This register can be used to select the capture edge for generating the capture event. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
0 | EDGE | Edge detect configuration for capture source
|
RW | 0 |
Address Offset | 0x0000 0044 | ||
Physical Address | 0x4000 2044 | Instance | 0x4000 2044 |
Description | Interrupt Mask. If a bit is set, then corresponding interrupt is un-masked. Un-masking the interrupt causes the raw interrupt to be visible in IIDX, as well as MIS. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
1 | EV1 | Channel 1 Event Interrupt Mask.
|
RW | 0 | |||||||||||
0 | EV0 | Channel 0 Event Interrupt Mask.
|
RW | 0 |
Address Offset | 0x0000 0048 | ||
Physical Address | 0x4000 2048 | Instance | 0x4000 2048 |
Description | Interrupt mask. This register selects interrupt sources which are allowed to pass from RIS to MIS when the corresponding bit-fields are set to 1. | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
1 | EV1 | Raw interrupt status for Channel 1 event. This bit is set to 1 when a capture event is received on Channel 1. This bit will be cleared when the bit in ICLR.EV1 is set to 1 or when the captured time value is read from the CH1CC8U register.
|
RO | 0 | |||||||||||
0 | EV0 | Raw interrupt status for Channel 0 event. This bit is set to 1 when a compare event occurs on Channel 0. This bit will be cleared. When the corresponding bit in ICLR.EV0 is set to 1. Or when a new compare value is written in CH0CC8U register
|
RO | 0 |
Address Offset | 0x0000 004C | ||
Physical Address | 0x4000 204C | Instance | 0x4000 204C |
Description | Masked interrupt status. This register is simply a bitwise AND of the contents of IMASK and RIS.*] registers. A flag set in this register can be cleared by writing 1 to the corresponding ICLR register bit. | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
1 | EV1 | Masked interrupt status for channel 1 event.
|
RO | 0 | |||||||||||
0 | EV0 | Masked interrupt status for channel 0 event.
|
RO | 0 |
Address Offset | 0x0000 0050 | ||
Physical Address | 0x4000 2050 | Instance | 0x4000 2050 |
Description | Interrupt set register. This register can used by software for diagnostics and safety checking purposes. Writing a 1 to a bit in this register will set the event and the corresponding RIS bit also gets set. If the corresponding IMASK bit is set, then the corresponding MIS register bit also gets set. | ||
Type | WO |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
1 | EV1 | Set Channel 1 event Interrupt.
|
WO | 0 | |||||||||||
0 | EV0 | Set Channel 0 event Interrupt.
|
WO | 0 |
Address Offset | 0x0000 0054 | ||
Physical Address | 0x4000 2054 | Instance | 0x4000 2054 |
Description | Interrupt clear register. This register allows software to clear interrupts. Writing a 1 to a bit in this register will clear the event and the corresponding RIS bit also gets cleared. If the corresponding IMASK bit is set, then the corresponding MIS register bit also gets cleared. | ||
Type | WO |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
1 | EV1 | Clears channel 1 event interrupt.
|
WO | 0 | |||||||||||
0 | EV0 | Clears channel 0 event interrupt.
|
WO | 0 |
Address Offset | 0x0000 0058 | ||
Physical Address | 0x4000 2058 | Instance | 0x4000 2058 |
Description | Interrupt mask set register. Writing a 1 to a bit in this register will set the corresponding IMASK bit. | ||
Type | WO |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
1 | EV1 | Set channel 1 event interrupt mask.
|
WO | 0 | |||||||||||
0 | EV0 | Set channel 0 event interrupt mask.
|
WO | 0 |
Address Offset | 0x0000 005C | ||
Physical Address | 0x4000 205C | Instance | 0x4000 205C |
Description | Interrupt mask clear register. Writing a 1 to a bit in this register will clear the corresponding IMASK bit. | ||
Type | WO |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
1 | EV1 | Clears Channel 1 event interrupt mask.
|
WO | 0 | |||||||||||
0 | EV0 | Clears Channel 0 event interrupt mask.
|
WO | 0 |
Address Offset | 0x0000 0060 | ||
Physical Address | 0x4000 2060 | Instance | 0x4000 2060 |
Description | Emulation control register. This register controls the behavior of the IP related to core halted input. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
0 | HALT | Halt control.
|
RW | 0 |
Address Offset | 0x0000 0064 | ||
Physical Address | 0x4000 2064 | Instance | 0x4000 2064 |
Description | Digital test bus control register. This register can be used to bring out IP internal signals to the pads for observation. 16 signals can be observed per select value. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||||||||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||||||||
3:0 | SEL | Digital test bus selection mux control. Non-zero select values output a 16 bit selected group of signals per value.
|
RW | 0x0 |
© 2015 - 2016. Texas Instruments | All Rights Reserved |