![]() |
![]() |
TI BLE5-Stack API Documentation
3.02.01.00
|
Data Structures | |
struct | gapBondMgrCBs_t |
Callback Registration Structure. More... | |
Typedefs | |
typedef void(* | pfnGapCB_t) (uint32_t event, void *pBuf, uintptr_t arg) |
typedef void(* | pfnGapConnEvtCB_t) (Gap_ConnEventRpt_t *pReport) |
typedef uint8_t(* | pfnGapDevPrivModeCB_t) (GAP_Peer_Addr_Types_t addrType, uint8_t *pAddr) |
GAP Device Privacy Mode Callback Function. | |
typedef void(* | pfnGapIdleCB_t) () |
GAP Idle Callback Function. | |
typedef uint8_t(* | pfnSuppCentAddrRes_t) (uint8_t *deviceAddr, GAP_Peer_Addr_Types_t addrType) |
Central Address Resolution (CAR) Support Callback Function. | |
typedef void(* pfnGapCB_t) (uint32_t event, void *pBuf, uintptr_t arg) |
GAP Callback function pointer type for the advertising and scan modules.
This callback will return GapAdv Event IDs from the advertising module, some of which can be masked with GapAdv_eventMaskFlags_t. See the respective event in GapAdv Event IDs for the type that pBuf should be cast to.
This callback will also return GapAdv Event IDs from the advertising module. See the respective event in GapAdv Event IDs for the type that pBuf should be cast to.
typedef void(* pfnGapConnEvtCB_t) ( Gap_ConnEventRpt_t *pReport) |
GAP Callback function pointer type for Connection Event notifications.
When registered via Gap_RegisterConnEventCb, this callback will return a pointer to a Gap_ConnEventRpt_t from the controller after each connection event