Zigbee Over-The-Air Firmware UpgradeΒΆ
- Z-Stack OTA Upgrade
- 1. Introduction
- 2. OTA Overview
- 2.1 OTA Theory of Operation
- 2.2 OTA Image Converter Applications
- 2.3 OtaServer PC Tool
- 2.4 Z-Stack Implementation of the OTA Upgrade Cluster for Client Device
- 2.5 Z-Stack Implementation of the OTA Upgrade Cluster for Server Device
- 3. Boot Image Manager (BIM)
- 4. OAD Image Header
- 5. Using the Sample OTA Applications
- 6. Adding Client Functionality to an Application
- 7. OTA Client Application Binary Usage
- TI Over-the-Air Download (OAD)