![]() |
Z-Stack API Reference
3.2.0
|
#include <zstackmsg.h>
Data Fields | |
zstackmsg_HDR_t | hdr |
zstack_bdbRepAddAttrCfgRecordDefaultToListReq_t * | pReq |
Send this message to the ZStack Thread to indicate the stack the default attribute reporting configuration for an attribute. This default configuration will be used if no Report Configuration command is issued to this device. This configuration will also be used when the device is instructed to return to its default configuration with a Report Configure command or Factory New Reset. If no Report Configuration command is received, this default configuration will be used when to report the attribute automatically if a bind to the cluster indicated is added. The command ID for this message is zstackmsg_CmdIDs_BDB_REP_ADD_ATTR_CFG_RECORD_DEFAULT_TO_LIST_REQ.
zstackmsg_HDR_t hdr |
message header
event field must be set to zstack_CmdIDs
Message command fields