![]() |
Z-Stack API Reference
3.2.0
|
#include <zstack.h>
Data Fields | |
zstack_ZdpStatus | status |
zstack_LongAddr_t | ieeeAddr |
uint16_t | nwkAddr |
uint8_t | startIndex |
uint8_t | n_assocDevList |
uint16_t * | pAssocDevList |
Structure to send a ZDO IEEE Address Response Indication.
zstack_LongAddr_t ieeeAddr |
64 bit IEEE address of source device
uint8_t n_assocDevList |
Number of associated devices in the list
uint16_t nwkAddr |
Network address of the responding device
uint16_t* pAssocDevList |
Array of (uint16_t) associated devices
uint8_t startIndex |
Starting index into the list of associated devices
zstack_ZdpStatus status |
Response status