![]() |
Z-Stack API Reference
3.2.0
|
#include <zstack.h>
Data Fields | |
uint32 | transID |
uint8 | extendedPANID [Z_EXTADDR_LEN] |
uint8 | nwkUpdateId |
uint8 | logicalChannel |
uint16 | PANID |
uint16 | nwkAddr |
Structure to send a Touchlink Target Network Join Request.
uint8 extendedPANID[Z_EXTADDR_LEN] |
IEEE address
uint8 logicalChannel |
Logical channel
uint16 nwkAddr |
Nwk address
uint8 nwkUpdateId |
Update identifier
uint16 PANID |
Network Pan ID
uint32 transID |
The inter-PAN transaction identifier field is 32-bits in length and specifies an identifier for the inter-PAN transaction