![]() |
Z-Stack API Reference
3.2.0
|
#include <zstack.h>
Data Fields | |
zstack_LogicalTypes | logicalType |
bool | complexDescAvail |
bool | userDescAvail |
uint8_t | apsFlags |
uint8_t | freqBand |
zstack_CapabilityInfo_t | capInfo |
uint16_t | manufacturerCode |
uint8_t | maxBufferSize |
uint16_t | maxInTransferSize |
zstack_ServerCapabilities_t | serverMask |
uint16_t | maxOutTransferSize |
uint32_t | descCap |
Structure for the ZDO Node Descriptor
uint8_t apsFlags |
(5 bits) Node Flags assigned for APS
zstack_CapabilityInfo_t capInfo |
MAC Capabilities
bool complexDescAvail |
Set if the Complex Descriptor is available
uint32_t descCap |
Descriptor capabilities
uint8_t freqBand |
(3 bits) Identifies node frequency band capabilities
zstack_LogicalTypes logicalType |
Device type
uint16_t manufacturerCode |
Manufacturer Code allocated by Zigbee Alliance
uint8_t maxBufferSize |
Maximum size of NPDU
uint16_t maxInTransferSize |
Maximum size of transfer up to 0x7FFF, reserved and shall be set to 0
uint16_t maxOutTransferSize |
(uint16_t) Maximum size of Transfer up to 0x7FFF
zstack_ServerCapabilities_t serverMask |
Server Capabilities
bool userDescAvail |
Set if the User Descriptor is available