![]() |
Z-Stack API Reference
3.2.0
|
#include <zstack.h>
Data Fields | |
gp_DataIndSecReq_t | SecReqHandling |
uint32 | timestamp |
uint8 | status |
int8 | Rssi |
uint8 | LinkQuality |
uint8 | SeqNumber |
sAddr_t | srcAddr |
uint16 | srcPanID |
uint8 | appID |
uint8 | GPDFSecLvl |
uint8 | GPDFKeyType |
bool | AutoCommissioning |
bool | RxAfterTx |
uint32 | SrcId |
uint8 | EndPoint |
uint32 | GPDSecFrameCounter |
uint8 | GPDCmmdID |
uint32 | MIC |
uint8 | GPDasduLength |
uint8 | GPDasdu [1] |
Structure to send a GP Data Indication.
uint8 appID |
The ApplicationID, corresponding to the received MPDU. ApplicationID 0x00 indicates the usage of the SrcID; ApplicationID 0x02 indicates the usage of the GPD IEEE address
bool AutoCommissioning |
The Auto-Commissioning sub-field, copied from the received GPDF
uint8 EndPoint |
The identifier of the GPD endpoint used in combination with the GPD IEEE address if ApplicationID = 0b010. If ApplicationID = 0b000 this parameter is ignored
uint8 GPDasdu[1] |
The sequence of octets forming the received GPD ASDU
uint8 GPDasduLength |
The number of octets in the received GPD ASDU
uint8 GPDCmmdID |
The identifier of the command, within the GP specification, which defines the application semantics of the ASDU
uint8 GPDFKeyType |
The security key type, which was successfully used for security processing the received MPDU
uint8 GPDFSecLvl |
The security level, corresponding to the received MPDU
uint32 GPDSecFrameCounter |
The security frame counter value used on transmission by the GPD entity from which the ASDU was received
uint8 LinkQuality |
The LQI delivered by the MAC on receipt of this frame
uint32 MIC |
The sequence of octets forming the MIC for the received GPD MPDU
int8 Rssi |
The RSSI delivered by the MAC on receipt of this frame
bool RxAfterTx |
The RxAfterTx sub-field, copied from the received GPDF
gp_DataIndSecReq_t SecReqHandling |
The data indication Handler
uint8 SeqNumber |
The sequence number from MAC header of the received MPDU
sAddr_t srcAddr |
The device address of the GPD entity from which the ASDU was received
uint32 SrcId |
The identifier of the GPD entity from which the ASDU was received
uint16 srcPanID |
The 16-bit PAN identifier of the GPD entity from which the ASDU was received
uint8 status |
Status code, as returned by dGP stub
uint32 timestamp |
The Timestamp delivered by the MAC on receipt of this frame