Z-Stack API Reference
3.2.0
|
#include <zstack.h>
Data Fields | |
uint8_t | logicalChannel |
uint16_t | panID |
zstack_LongAddr_t | extendedPANID |
uint16_t | chosenParent |
uint8_t | parentDepth |
uint8_t | stackProfile |
Structure to send a Device Join Requst.
uint16_t chosenParent |
Short address of parent device chosen to join
zstack_LongAddr_t extendedPANID |
64 bit extended PAN ID, use all 0xFF if don't care
uint8_t logicalChannel |
Channel where the PAN is located
uint16_t panID |
ID of the PAN to join
uint8_t parentDepth |
Depth of the parent
uint8_t stackProfile |
Stack profile of the network to join