![]() |
Z-Stack API Reference
3.2.0
|
#include <zstack.h>
Data Fields | |
bool | panCoord |
bool | ffd |
bool | mainsPower |
bool | rxOnWhenIdle |
bool | security |
Structure defines the Capabilities Information bit field.
bool ffd |
True if the device is a full function device (FFD)
bool mainsPower |
True if the device is mains powered
bool panCoord |
True if the device is a PAN Coordinator
bool rxOnWhenIdle |
True if the device's RX is on when the device is idle
bool security |
True if the device is capable of sending and receiving secured frames