Z-Stack API Reference
3.2.0
|
#include <zstack.h>
Data Fields | |
uint32_t | bdbSecondaryChannelSet |
bool | has_bdbSecondaryChannelSet |
uint32_t | bdbPrimaryChannelSet |
bool | has_bdbPrimaryChannelSet |
uint16_t | bdbCommissioningGroupID |
bool | has_bdbCommissioningGroupID |
uint8_t | bdbScanDuration |
bool | has_bdbScanDuration |
bool | bdbJoinUsesInstallCodeKey |
bool | has_bdbJoinUsesInstallCodeKey |
uint8_t | bdbTrustCenterNodeJoinTimeout |
bool | has_bdbTrustCenterNodeJoinTimeout |
bool | bdbTrustCenterRequireKeyExchange |
bool | has_bdbTrustCenterRequireKeyExchange |
uint8_t | bdbTCLinkKeyExchangeAttemptsMax |
bool | has_bdbTCLinkKeyExchangeAttemptsMax |
uint8_t | bdbTCLinkKeyExchangeMethod |
bool | has_bdbTCLinkKeyExchangeMethod |
Structure to send a BDB Set Attributes Request. Each config field has 2 parts to it, the actual value field and its "has_" field. The "has_" field must be set to "true" for the value field to be valid. For example, the pollRate field is valid only if the has_pollRate field is set to true.
uint16_t bdbCommissioningGroupID |
Group ID for Finding and Binding
bool bdbJoinUsesInstallCodeKey |
Is install codes mandated for joining devices? (ZC only)
uint32_t bdbPrimaryChannelSet |
Primary Channel Set
uint8_t bdbScanDuration |
Scan Duration
uint32_t bdbSecondaryChannelSet |
Secondary Channel Set
uint8_t bdbTCLinkKeyExchangeAttemptsMax |
Maximum number of attempts to join the same network will be done before give up (ZR/ZED only)
uint8_t bdbTCLinkKeyExchangeMethod |
Standard TCLK or CBKE (ZR/ZED only)
uint8_t bdbTrustCenterNodeJoinTimeout |
Timeout to allow joining devices to perform TCLK exchange (ZC only)
bool bdbTrustCenterRequireKeyExchange |
Is mandated to perform TCLK exchange for joining devices? (ZC only)
bool has_bdbCommissioningGroupID |
Set to true if bdbCommissioningGroupID is available, false if not
bool has_bdbJoinUsesInstallCodeKey |
Set to true if bdbJoinUsesInstallCodeKey is available, false if not
bool has_bdbPrimaryChannelSet |
Set to true if bdbPrimaryChannelSet is available, false if not
bool has_bdbScanDuration |
Set to true if bdbScanDuration is available, false if not
bool has_bdbSecondaryChannelSet |
Set to true if bdbSecondaryChannelSet is available, false if not
bool has_bdbTCLinkKeyExchangeAttemptsMax |
Set to true if bdbTCLinkKeyExchangeAttemptsMax is available, false if not
bool has_bdbTCLinkKeyExchangeMethod |
Set to true if bdbTCLinkKeyExchangeMethod is available, false if not
bool has_bdbTrustCenterNodeJoinTimeout |
Set to true if bdbTrustCenterNodeJoinTimeout is available, false if not
bool has_bdbTrustCenterRequireKeyExchange |
Set to true if bdbTrustCenterRequireKeyExchange is available, false if not