![]() |
Z-Stack API Reference
3.2.0
|
#include <zstack.h>
Data Fields | |
uint8_t | endpoint |
uint16_t | cluster |
uint16_t | attrID |
uint16_t | minReportInt |
uint16_t | maxReportInt |
uint8_t | reportableChange [8] |
Structure to send a BDB Reportorting Attribute Configure Record Default Request.
uint16_t attrID |
Attribute ID
uint16_t cluster |
Cluster
uint8_t endpoint |
Endpoint
uint16_t maxReportInt |
Value for maximum reportable interval. If no change to the attribute is done, this is the period with which the attribute is reported.
uint16_t minReportInt |
Value for minimum reportable interval
uint8_t reportableChange[8] |
Attribute value that is the delta change to trigger a report