![]() |
Z-Stack API Reference
3.2.0
|
#include <zstack.h>
Data Fields | |
uint32_t | bdbSecondaryChannelSet |
uint32_t | bdbPrimaryChannelSet |
uint16_t | bdbCommissioningGroupID |
uint8_t | bdbCommissioningStatus |
uint8_t | bdbCommissioningMode |
uint8_t | bdbNodeCommissioningCapability |
uint8_t | bdbScanDuration |
bool | bdbNodeIsOnANetwork |
bool | bdbJoinUsesInstallCodeKey |
uint8_t | bdbTrustCenterNodeJoinTimeout |
bool | bdbTrustCenterRequireKeyExchange |
uint8_t | bdbNodeJoinLinkKeyType |
uint8_t | bdbTCLinkKeyExchangeAttempts |
uint8_t | bdbTCLinkKeyExchangeAttemptsMax |
uint8_t | bdbTCLinkKeyExchangeMethod |
Structure to send a BDB Get Attribute Request. This is used to retrieve the attributes currently set for bdb commissioning procedures.
uint16_t bdbCommissioningGroupID |
Group ID for Finding and Binding
uint8_t bdbCommissioningMode |
Current commissioning methods in progress (read only)
uint8_t bdbCommissioningStatus |
Commissioning status from last call. Is suggested to use icall notifications instead
bool bdbJoinUsesInstallCodeKey |
Is install codes mandated for joining devices? (ZC only)
uint8_t bdbNodeCommissioningCapability |
Commissioning capabilities (read only)
bool bdbNodeIsOnANetwork |
Is the device commissioned to a network (read only)
uint8_t bdbNodeJoinLinkKeyType |
LinkKey used by the joining device (read only)(ZR/ZED only)
uint32_t bdbPrimaryChannelSet |
Primary Channel Set
uint8_t bdbScanDuration |
Scan Duration
uint32_t bdbSecondaryChannelSet |
Secondary Channel Set
uint8_t bdbTCLinkKeyExchangeAttempts |
Number of attempts to perform association in the current network (read only) (ZR/ZED only)
uint8_t bdbTCLinkKeyExchangeAttemptsMax |
Maximum number of attempts to join the same network will be done before giveup (ZR/ZED only)
uint8_t bdbTCLinkKeyExchangeMethod |
Standard TCLK or CBKE (ZR/ZED only)
uint8_t bdbTrustCenterNodeJoinTimeout |
Timeout to allow joining devices to perform TCLK exchange (ZC only)
bool bdbTrustCenterRequireKeyExchange |
Is mandated to perform TCLK exchange for joining devices? (ZC only)