![]() |
Z-Stack API Reference
3.2.0
|
#include <zstack.h>
Data Fields | |
uint8_t | endpoint |
The endpoint that will receive messages sent to the group in the group field. | |
uint16_t | groupID |
This is the group ID that is set over the air. | |
uint8_t | n_name |
length of "name" | |
uint8_t * | pName |
pointer to the Human readable "name" of group | |
Structure to send an APS Add Group Request.