TI-OpenThread Native OAD

Warning

This is an experimental version of the TI-OpenThread Stack OAD, and is currently experiencing ongoing development. Expect future versions to change.

A common OAD process can be seen as two very distinct phases: notification and transport of new images to a device, and updating into a newly downloaded image. First phase will inherently be different from protocol to protocol, as it will depend on protocol specific details. However, the second phase is protocol invariant and is based on a common architecture across protocols.

TI-OpenThread Stack supports a native OAD process, which is a TI-OpenThread Stack proprietary design and implementation. The Thread specification does not specify any standard process for OAD, which means any implementation of a native OAD process will be proprietary.

BIM is used as the common architecture for handling and updating new images on a device. Since BIM is a protocol invariant architecture, an OAD-enabled Thread Application can be transported over an another protocol that is OAD compatible, such as BLE. Refer to the Boot Image Manager (BIM) Chapter for more details.

For more information on the specifics of BLE OAD, consult the BLE User’s Guide.

System Overview

As detailed in Section OAD Topology Overview, an OAD exchange happens between two devices: an OAD Target and an OAD Distributor. The OAD Target is the device that receives the candidate images over the air, while the OAD Distributor notifies the OAD Target of new, available images and supplies the firmware update.

Note

TI-OpenThread Stack only supports off-chip OAD, and therefore an external flash is required. During off-chip OAD, the candidate image is stored on the external flash and subsequently loaded into the internal flash.

For TI-OpenThread Stack, the Target device is a Thread device which can both be an FTD or an MTD. This also includes SEDs. The Distributor must also be a Thread device connected to the same Thread Network as the Target device. That means the connection between the Distributor and the Target device cannot go off-mesh.

It is assumed that only a single Distributor exists on a Thread Network. However, multiple Distributors can co-exist in the same Thread Network. If a Target device were to receive multiple image notifications from different Distributors, it is up to the Target device to decide which image notification it accepts and rejects.

A candidate image is split into blocks, and each image block is transferred individually in sequence. The size of each block can be configured, with a default value of 128 bytes.

When a candidate image has been downloaded, the Target device does a system reset and BIM performs the actual procedure of updating into that image. Refer to Chapter Boot Image Manager (BIM) for more details on the update procedure.

../_images/ditaa-48e74a8369e53a303fc41b5a1992ed055a580d32.png

OAD CoAP

The Constrained Application Protocol (CoAP) is used as the means of communication between the Distributor and the Target device. This includes registering new Target devices, notifying Taget devices of new candidate images, as well as the actual transport of candidate images.

Both the Distributor and the Target device acts as CoAP servers, with both devices exposing a set of CoAP resources denoted by URI. Each resource has a corresponding request and response message pair, for which a CoAP Client will send a request message to a given resource and the CoAP Server will respond with a response message.

Table 4. provides an overview of which CoAP resources are available for which OAD device. Table 5. provides an overview what kind of requests and responses are expected for each CoAP resource.

Ideally, CoAP Block-Wise Transfers would be used for transfer of firmware images, as it provides a minimal way of transferring large data in a block-wise fashion. However, OpenThread does not implement Block-Wise Transfers for its CoAP implementation, and subsequently is not used in the OAD protocol implementation for TI-OpenThread.

Table 4. OAD CoAP resource overview
OAD Device CoAP URI Description
Distributor oad/reg Used by Target devices to register its ULA to the Distributor. This is only used if the Distributor does not any other means to acquire the ULA of the Target device.
oad/img Used by Target devices to request a specific image block for a specific image.
Target oad/fwv Used for the Distributor to acquire information of which software version and BIM version the Target device is currently running.
oad/ntf Used to notify Target devices that new images are available at the Distributor.
Table 5. OAD CoAP message overview
CoAP URI Message Description
oad/reg Request Non-confirmable PUT request. Content is the ML-EID of the sending Target device.
Response No response.
oad/img Request Confirmable GET request. Content is a block number for a specific image.
Response Piggybacked response. Content is the requested image block.
oad/fwv Request Confirmable GET request.
Response Piggybacked response. Content is the current software version and BIM version running on the Target device.
oad/ntf Request Confirmable PUT request. Content is information about the new available image.
Response Piggybacked response. Content is image accepted or rejected.

OAD Protocol

The OAD protocol for TI-OpenThread is a proprietary protocol, and consists of the following steps:

Note

For all the sequence diagrams in this section, messages going between the CoAP Server and Client are messages which are transmitted on the Thread Network. Any required hops between additional Thead devices are omited.

  1. (Optional) Target device registers its Unique Local Address to the Distributor.

    Target devices sends a Register Request message with the oad/reg URI to the multicast address ff03::2. The contents of the request is the ML-EID of the Target device, represented in bytes. On reception of the request, the Distributor stores the ULA of the Target device. This step is necessary if the Distributor does not have knowledge of all End Devices in the Thread Network.

@startuml
hide footbox

participant Target as target
participant "CoAP Client" as target_coap
participant "CoAP Server" as distr_coap
participant Distributor as distr

activate distr
activate target

target -> target_coap : Register request
activate target_coap

group Multicast ff03::2

    target_coap -> distr_coap : NON [0xaf6] PUT /oad/reg\nContent {Target ULA}
    deactivate target_coap
    activate distr_coap

end

distr_coap -> distr : CoAP Server callback
deactivate distr_coap

@enduml

Figure 70. Target registers its ULA to the Distributor

  1. (Optional) Distributor acquires Firmware Version information from Target device.

    Distributor sends a Firmware Version Request message with the oad/fwv URI to the unicast address of a Target device. The response from the Target device contains information about its current software version and BIM version.

    The software version is a four character string which keeps track of the application and stack revision contained in the image. Refer to Software version for more information. The BIM version is a byte, which is used to determine if images are compatible with BIM that is running on the device. Refer to BIM Version for more information.

    The response is on the format "sv:XXXX bv:YY", where XXXX is the software version, and YY is the BIM version byte in string representation. Note the space between the software version and the BIM version.

@startuml
hide footbox

participant Distributor as distr
participant "CoAP Client" as distr_coap
participant "CoAP Server" as target_coap
participant Target as target

activate distr
activate target

distr -> distr_coap : Firmware Version request
activate distr_coap

distr_coap -> target_coap : CON [0x102] GET /oad/fwv
activate target_coap

target_coap -> target : CoAP Server callback

target -> target_coap : Firmware Version response

target_coap -> distr_coap : ACK [0x102] 2.05 Content "sv:0001 bv:03"
deactivate target_coap

distr_coap -> distr : CoAP Client callback
deactivate distr_coap

@enduml

Figure 71. Distributor retrieves firmware information from Target

  1. Distributor notifies Target devices that a new firmware image is available.

    When the Distributor has a new candidate image, it notifies Target devices depending on their Firmware Version information. Distributor sends Image Notification requests with the oad/ntf URI to the unicast addresses of a Target devices. Distributor decides when to notify Target devices and in which order.

    The request contains information about the new candidate image, such as software and BIM compability, and firmware image type and size. Target device responds with either an image accept or reject based on the provided information.

@startuml
hide footbox

participant Distributor as distr
participant "CoAP Client" as distr_coap
participant "CoAP Server" as target_coap
participant Target as target

activate distr
activate target

distr -> distr_coap : Image Notify request
activate distr_coap

distr_coap -> target_coap : CON [0x341] PUT /oad/ntf\nContent {Image information}
activate target_coap

target_coap -> target : CoAP Server callback

target -> target_coap : Image Notify response

alt Image accepted

    target_coap -> distr_coap : ACK [0x341] 2.05 Content "Accept"

else Image rejected

    target_coap -> distr_coap : ACK [0x341] 2.05 Content "Reject"
    deactivate target_coap

end


distr_coap -> distr : CoAP Client callback
deactivate distr_coap

@enduml

Figure 72. Distributor notifies Target of new candidate image

  1. Target device starts the download process.

    Only if the candidate image is accepted will the Target device initate the download process. Target device sends Image Block requests with the oad/img URI to the unicast address of the Distributor. The request describes which a block from the image, denoted by a block number.

    Blocks are requested in a sequential order, and the Target device keeps track of what the current block number is. Only when the current block number has been successfully downloaded will the Target device request the next block. Block are stored in external flash when downloaded.

    What is important to note is that the Target device decides when blocks are requested and at which rate. This means the download process is completely driven by the Target device. The Distributor does not put any constraints on Target devices how fast the download must occur. As long as the candidate image is available, the download process can take as long time as the Target device wants.

@startuml
hide footbox

participant Target as target
participant "CoAP Client" as target_coap
participant "CoAP Server" as distr_coap
participant Distributor as distr

activate target
activate distr

loop For all Image Blocks

    target -> target_coap : Image Block request
    activate target_coap

    target_coap -> distr_coap : CON [0x7a8] GET /oad/img\nContent {Block number}
    activate distr_coap

    distr_coap -> distr : CoAP Server callback

    distr -> distr_coap : Image Block response

    distr_coap -> target_coap : ACK [0x7a8] 2.05\nContent {Block data}
    deactivate distr_coap

    target_coap -> target : CoAP Client callback
    deactivate target_coap

end

@enduml

Figure 73. Target requests a single image block from Distributor

  1. On download complete, Target device updates the firmware image.

    When all blocks have been successfully downloaded, the candidate image is now stored in external flash on the Target device in its entirety. The candidate image is verified, that is the integrity of the image is OK; if the image is valid, it is marked as the new image to be booted in. Else, the image is rejected.

    Target device reset itself and BIM copies the new image to the internal flash. If an error occurs during the copy procedure, BIM switches back to a factory image. Refer to Section BIM for Off-Chip OAD for more details about the BIM procedure.

OAD Pause and Resume

Since the download process of the image is driven by the Target device, it has the ability to explicitly pause and resume download. The key difference between pausing a download and setting the rate between each block request, is that pausing is indefinite until an explicit resume is invoked. Setting the request rate only changes the waiting period until the next block request.

The Target device can also be paused if the device loses network connection or loses power. When the device restores the network connection or regains power, it has the ability to resume the download process and pick up from where it left off.

From the Distributor’s point of view, there is no difference if the Target device is paused or not. The Distributor only responds whenever a block requests is received, which can be sent at any given time.

OAD Abort

Whenever the Target device sends a block request, there always a risk that either the block request never reaches the Distributor, or the response never reaches back to the Target device. Thread takes care of retransmissions at the MAC layer, while CoAP takes care of retransmissions at the transport layer.

If retransmissions are not sufficent, or if the Distributor is simply unavailable, then the Target device will eventually reach a maximum number of retransmissions and the download is aborted. However, the Target device can later try and resume the download if appropriate.

The number of retransmissions CoAP sends for confirmable messages are configurable at the application level, with a default count of four.

Figure 74. shows a sequence diagram of a block request which initially succeeds, but the Distributer suddenly becomes unavailable. The subsequent block request now does not result in any response and the target Device starts sending retransmissions of the block request. After the number of retransmits hits maximum, the Target device aborts the download.

@startuml
hide footbox

participant Target as target
participant "CoAP Client" as target_coap
participant "CoAP Server" as distr_coap
participant Distributor as distr

activate target
activate distr

target -> target_coap : Image Block request
activate target_coap

target_coap -> distr_coap : CON [0x558] GET /oad/img\nContent {Block number}
activate distr_coap

distr_coap -> distr : CoAP Server callback

distr -> distr_coap : Image Block response

distr_coap -> target_coap : ACK [0x558] 2.05\nContent {Block data}
deactivate distr_coap

target_coap -> target : CoAP Client callback
deactivate target_coap

...

distr <--] : Becomes unavailable
deactivate distr

target -> target_coap : Image Block request
activate target_coap

target_coap ->x distr_coap : CON [0xC30] GET /oad/img\nContent {Block number}
|||
target_coap ->x distr_coap : CON [0xC30] GET /oad/img\nContent {Block number}
...N number of retries ...
target_coap ->x distr_coap : CON [0xC30] GET /oad/img\nContent {Block number}

note right of target_coap: Maximum number retries met

target_coap -> target : OAD Abort
deactivate target_coap

@enduml

Figure 74. OAD image download abort

OAD Application Usage

An application developer wishing to use the TI-OpenThread OAD solution will not need to worry about implementing the OAD state machine, but can instead just include the OAD module. The OAD module implements the OAD state machine, which is defined by the OAD protocol.

The OAD state machine differs between the Target device and Distributor, and therefore the OAD module will be different for both OAD devices. In addition, the architectural requirements for the Target device and the Distributor are different, which will be highlighted in the subsequent sections.

Warning

There currently does not exist an OAD module for the OAD Distributor.

The size of the image block sent from the Distributor to the Target device can be configured, with a default size of 128 bytes. The define OAD_BLOCK_SIZE configures the block size, and is set independently in both the Target device application and the Distributor application.

Note

The OAD_BLOCK_SIZE define must be set to the same value for both the Target device and Distributor application, since block size negotiation is not supported.


OAD Target Device Application

A Target device will in most use cases be a single-chip, Thread-only device. In other words, the application layer and OpenThread runs on the same processor.

Note

The OAD module for Target devices only supports single-chip, Thread-only platforms.

The OAD module for the Target device is provided as part of the TI-OpenThread environment, and implements the OAD protocol and the off-chip storage handling. The module is based on the OpenThread CoAP implementation. Figure 75. describes the OAD state machine for the Target device.

@startuml

hide empty description

state "Idle" as idle
state "Image Download" as img_dl
state "Image Validate" as img_val
state "BIM" as bim

[*] -right-> idle : Register with\nDistributor

idle -right-> img_val : Image\navailable
idle -down-> img_dl : Network recovery,\nOAD resume

img_val : Image notification\nand validation
img_val --> idle : Image\nrejected
img_val --> img_dl : Image\naccepted

img_dl : Download image\nprocedure
img_dl -up-> idle : Network failure,\nOAD abort
img_dl --> img_dl : Block\nrequest
img_dl --> bim : Download\ncomplete

bim : Firmware update
bim -left-> [*]

@enduml

Figure 75. OAD Target state diagram

Target Application Interface

The OAD module for the Target device exposes the following API.

/**
 * @brief  Initializes the OAD module on network connection event
 * @return None
 */
void OAD_open(void);

/**
 * @brief  Close the OAD module
 * @return None
 */
void OAD_close(void);

/**
 * @brief  Abort firmware download on transmission error
 * @return None
 */
void OAD_abort(void);

/**
 * @brief  Download resume on service recovery or reboot
 * @return None
 */
void OAD_resume(void);

/**
 * @brief  Pause OAD module, if valid download in progress
 * @return None
 */
void OAD_pause(void);

/**
 * @brief  A function to process the OAD events
 * @return None
 */
void OAD_processQueue(void);

OAD Distributor Application

Since the Distributor has to in some way acquire new candidate images (either via other IP network, or direct links with an operator), the most natural architecture would be an NCP. In addition, the Distributor will likely need to store multiple candidate images, which puts higher memory requirements on the device. The application layer would run on a host MCU, while Thread features run on the SoC.

Since the application layer of the Distributor would in most cases run on some host, the CoAP implementation no longer depends on the OpenThread implementation. Rather, any CoAP implementation can be used that is compatible with the host MCU environment.

Warning

There currently does not exist an OAD module for the OAD Distributor.

Even though there does not exist an OAD module for the Distributor, Figure 76. describes the OAD state machine.

@startuml

hide empty description

state "Idle" as idle
state "Send Notification" as send_ntf
state "Send Block" as send_block
state "Update Target" as update_target

[*] --> idle

idle -left-> send_ntf : New image\navailable
idle -right-> send_block : Block\nrequest
idle -down-> update_target : Register\nnotify

send_ntf : Notify Target\ndevices
send_ntf --> idle : No response
send_ntf --> update_target : Image accepted\nor rejected

send_block : Send a block\nto Target
send_block --> idle : No response
send_block --> update_target : Block send\ncomplete

update_target : Update Target\nlist
update_target --> idle : Update\ncomplete

@enduml

Figure 76. OAD Distributor state diagram


CoAP Message Layout

The following tables describes the content layout of the various CoAP messages.

Table 6. Register request content
Field Size (in bytes) Description
Unique Local Address 16 An IPv6 Unique Local Address of the Target device
Table 7. Firmware Version response content
Field Size (in bytes) Description
Software Version 7 String representation on the format sv:XXXX, where XXXX is a four character string which indicates the Software Version
Divider 1 Dummy character to separate the Software and BIM Version, defaults to space character
BIM Version 5 String representation on the format bv:YY, where YY is a string representation of a byte number which indicates the BIM Version
Reserved 19 Default is set to zero
Table 8. Image Notify request content
Field Size (in bytes) Description
Image ID 1 Identifier for which image the notification corresponds to
OAD Image ID 8 Unique number to identify the start of an OAD image
BIM Version 1 Version required to support image format
Meta Version 1 Version of image header contained in image
Image Copy Status 1 Status of whether the Image has been copied or not
CRC Status 1 Status of the CRC check
Image Type 1 Type of image, e.g. Application or Factory image
Image Number 1 Distinguish between multiple images within a technology
Image Length 4 The total length of the image including header
Software Version 4 Software version of the image
Table 9. Image Notify Response content
Field Size (in bytes) Description
Image ID 1 Identifier for which image the notification corresponds to
Status 1 Status indicating if the notification request was accepted or rejected
Table 10. Image Block Request content
Field Size (in bytes) Description
Image ID 1 Identifier for which image the block corresponds to
Block Number 2 Which block to download
Total Blocks 2 Total number of blocks the image consists of
Table 11. Image Block Response content
Field Size (in bytes) Description
Image ID 1 Identifier for which image the block corresponds to
Block Number 2 Which block to download
Data OAD_BLOCK_SIZE Block data, where its size is configurable

TI-OpenThread OAD Examples

The SimpleLink CC26x2 SDK contains example applications which both are OAD-enabled and can perform OAD operations. Following is a description of available example applications and how to use them.

Warning

There currently does not exist any example application for an OAD Distributor.

Some of the OAD examples can manually revert back to a factory image, if a factory image is present. See the following steps for how to revert to the factory image.

  1. Hold down the left button on the CC26x2 LaunchPad.

  2. While holding down the left button, press the reset button.

    • On boot, the application will check the pin state and jump to the invalidate routine.

The process for invaliding the current image is as follows:

  • The application corrupts the CRC status field in the OAD Image Header by flipping a bit.
  • The application reboots the device.
  • The BIM will search for valid images, and since no new downloads have been performed, it will not find any.
  • At this point as a failsafe, the BIM will revert the factory image.

Note

The application should check that a valid factory image is present before invalidating itself. It can do so by ensuring there is valid metadata in external flash page 0. See OAD External Flash Image Header.

OAD CLI

The OAD CLI example is equivalent to the CLI example, with the addition of being OAD-enabled. That means the generated image file can be used as a candidate image for an OAD exchanage.

The example does not display any usage of the OAD module. It is simply an OAD-enabled Thread project. Refer to Section Create a TI-OpenThread OAD Image for how to make existing Thread projects downloadable.

The OAD CLI example does support reverting back to a factory image.

Door Lock OAD

The Door Lock OAD example is a modified version of the Door Lock example, which implements an OAD Target device ontop of the existing example. The example gives an example usage of the OAD module, and how one would implement an OAD Target device.

The Door Lock OAD example does not support reverting back to a factory image.