#include <rf_ieee_cmd.h>
Data Fields | |
uint8_t | nTxAck |
Total number of transmitted ACK frames. More... | |
uint8_t | nRxBeacon |
Number of received beacon frames. More... | |
uint8_t | nRxData |
Number of received data frames. More... | |
uint8_t | nRxAck |
Number of received acknowledgement frames. More... | |
uint8_t | nRxMacCmd |
Number of received MAC command frames. More... | |
uint8_t | nRxReserved |
Number of received frames with reserved frame type. More... | |
uint8_t | nRxNok |
Number of received frames with CRC error. More... | |
uint8_t | nRxIgnored |
Number of frames received that are to be ignored. More... | |
uint8_t | nRxBufFull |
Number of received frames discarded because the Rx buffer was full. More... | |
int8_t | lastRssi |
RSSI of last received frame. More... | |
int8_t | maxRssi |
Highest RSSI observed in the operation. More... | |
uint8_t | __dummy0 |
ratmr_t | beaconTimeStamp |
Time stamp of last received beacon frame. More... | |
uint8_t rfc_ieeeRxOutput_s::__dummy0 |
ratmr_t rfc_ieeeRxOutput_s::beaconTimeStamp |
Time stamp of last received beacon frame.
int8_t rfc_ieeeRxOutput_s::lastRssi |
RSSI of last received frame.
int8_t rfc_ieeeRxOutput_s::maxRssi |
Highest RSSI observed in the operation.
uint8_t rfc_ieeeRxOutput_s::nRxAck |
Number of received acknowledgement frames.
uint8_t rfc_ieeeRxOutput_s::nRxBeacon |
Number of received beacon frames.
uint8_t rfc_ieeeRxOutput_s::nRxBufFull |
Number of received frames discarded because the Rx buffer was full.
uint8_t rfc_ieeeRxOutput_s::nRxData |
Number of received data frames.
uint8_t rfc_ieeeRxOutput_s::nRxIgnored |
Number of frames received that are to be ignored.
uint8_t rfc_ieeeRxOutput_s::nRxMacCmd |
Number of received MAC command frames.
uint8_t rfc_ieeeRxOutput_s::nRxNok |
Number of received frames with CRC error.
uint8_t rfc_ieeeRxOutput_s::nRxReserved |
Number of received frames with reserved frame type.
uint8_t rfc_ieeeRxOutput_s::nTxAck |
Total number of transmitted ACK frames.