#include <rf_ble_cmd.h>
Data Fields | |
uint8_t | size |
Number of while list entries. Used in the first entry of the list only. More... | |
struct { | |
uint8_t bEnable:1 | |
1 if the entry is in use, 0 if the entry is not in use More... | |
uint8_t addrType:1 | |
The type address in the entry – public (0) or random (1) More... | |
uint8_t bWlIgn:1 | |
1 if the entry is to be ignored by a scanner if the AdvDataInfo field is not present, 0 otherwise. Used to mask out entries that have already been scanned and reported. More... | |
uint8_t __pad0__:1 | |
uint8_t bPrivIgn:1 | |
1 if the entry is to be ignored as part of a privacy algorithm, 0 otherwise More... | |
} | conf |
uint16_t | address |
Least significant 16 bits of the address contained in the entry. More... | |
uint32_t | addressHi |
Most significant 32 bits of the address contained in the entry. More... | |
uint8_t rfc_bleWhiteListEntry_s::__pad0__ |
uint16_t rfc_bleWhiteListEntry_s::address |
Least significant 16 bits of the address contained in the entry.
uint32_t rfc_bleWhiteListEntry_s::addressHi |
Most significant 32 bits of the address contained in the entry.
uint8_t rfc_bleWhiteListEntry_s::addrType |
The type address in the entry – public (0) or random (1)
uint8_t rfc_bleWhiteListEntry_s::bEnable |
1 if the entry is in use, 0 if the entry is not in use
uint8_t rfc_bleWhiteListEntry_s::bPrivIgn |
1 if the entry is to be ignored as part of a privacy algorithm, 0 otherwise
uint8_t rfc_bleWhiteListEntry_s::bWlIgn |
1 if the entry is to be ignored by a scanner if the AdvDataInfo field is not present, 0 otherwise. Used to mask out entries that have already been scanned and reported.
struct { ... } rfc_bleWhiteListEntry_s::conf |
uint8_t rfc_bleWhiteListEntry_s::size |
Number of while list entries. Used in the first entry of the list only.