#include <rf_ble_cmd.h>
Data Fields | |
struct { | |
uint16_t channel:6 | |
The channel on which the packet was received, provided channel is in the range 0–39; otherwise 0x3F. More... | |
uint16_t bIgnore:1 | |
1 if the packet is marked as ignored, 0 otherwise More... | |
uint16_t bCrcErr:1 | |
1 if the packet was received with CRC error, 0 otherwise More... | |
uint16_t phyMode:2 | |
The PHY on which the packet was received 0: 1 Mbps 1: 2 Mbps 2: Coded, S = 8 (125 kbps) 3: Coded, S = 2 (500 kbps) More... | |
} | status |
uint16_t rfc_ble5RxStatus_s::bCrcErr |
1 if the packet was received with CRC error, 0 otherwise
uint16_t rfc_ble5RxStatus_s::bIgnore |
1 if the packet is marked as ignored, 0 otherwise
uint16_t rfc_ble5RxStatus_s::channel |
The channel on which the packet was received, provided channel is in the range 0–39; otherwise 0x3F.
uint16_t rfc_ble5RxStatus_s::phyMode |
The PHY on which the packet was received
0: 1 Mbps
1: 2 Mbps
2: Coded, S = 8 (125 kbps)
3: Coded, S = 2 (500 kbps)
struct { ... } rfc_ble5RxStatus_s::status |