CC26xx Driver Library
rfc_CMD_SYNC_STOP_RAT_s Struct Reference

Synchronize and Stop Radio Timer Command. More...

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0809. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More...
 
condition
 
uint16_t __dummy0
 
ratmr_t rat0
 The returned RAT timer value corresponding to the value the RAT would have had when the RTC was zero. More...
 

Detailed Description

Synchronize and Stop Radio Timer Command.

Field Documentation

uint16_t rfc_CMD_SYNC_STOP_RAT_s::__dummy0
uint8_t rfc_CMD_SYNC_STOP_RAT_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

uint16_t rfc_CMD_SYNC_STOP_RAT_s::commandNo

The command ID number 0x0809.

struct { ... } rfc_CMD_SYNC_STOP_RAT_s::condition
uint8_t rfc_CMD_SYNC_STOP_RAT_s::nSkip

Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...

uint8_t rfc_CMD_SYNC_STOP_RAT_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

rfc_radioOp_t* rfc_CMD_SYNC_STOP_RAT_s::pNextOp

Pointer to the next operation to run after this operation is done.

ratmr_t rfc_CMD_SYNC_STOP_RAT_s::rat0

The returned RAT timer value corresponding to the value the RAT would have had when the RTC was zero.

uint8_t rfc_CMD_SYNC_STOP_RAT_s::rule

Condition for running next command: Rule for how to proceed.

ratmr_t rfc_CMD_SYNC_STOP_RAT_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

struct { ... } rfc_CMD_SYNC_STOP_RAT_s::startTrigger

Identification of the trigger that starts the operation.

uint16_t rfc_CMD_SYNC_STOP_RAT_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

uint8_t rfc_CMD_SYNC_STOP_RAT_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

uint8_t rfc_CMD_SYNC_STOP_RAT_s::triggerType

The type of trigger.