IEEE 802.15.4 CCA and RSSI Information Request Command. More...
#include <rf_ieee_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x2403. More... | |
int8_t | currentRssi |
The RSSI currently observed on the channel. More... | |
int8_t | maxRssi |
The maximum RSSI observed on the channel since Rx was started. More... | |
struct { | |
uint8_t ccaState:2 | |
Value of the current CCA state 0: Idle 1: Busy 2: Invalid. More... | |
uint8_t ccaEnergy:2 | |
Value of the current energy detect CCA state 0: Idle 1: Busy 2: Invalid. More... | |
uint8_t ccaCorr:2 | |
Value of the current correlator based carrier sense CCA state 0: Idle 1: Busy 2: Invalid. More... | |
uint8_t ccaSync:1 | |
Value of the current sync found based carrier sense CCA state 0: Idle 1: Busy. More... | |
} | ccaInfo |
IEEE 802.15.4 CCA and RSSI Information Request Command.
uint8_t rfc_CMD_IEEE_CCA_REQ_s::ccaCorr |
Value of the current correlator based carrier sense CCA state
0: Idle
1: Busy
2: Invalid.
uint8_t rfc_CMD_IEEE_CCA_REQ_s::ccaEnergy |
Value of the current energy detect CCA state
0: Idle
1: Busy
2: Invalid.
struct { ... } rfc_CMD_IEEE_CCA_REQ_s::ccaInfo |
uint8_t rfc_CMD_IEEE_CCA_REQ_s::ccaState |
Value of the current CCA state
0: Idle
1: Busy
2: Invalid.
uint8_t rfc_CMD_IEEE_CCA_REQ_s::ccaSync |
Value of the current sync found based carrier sense CCA state
0: Idle
1: Busy.
uint16_t rfc_CMD_IEEE_CCA_REQ_s::commandNo |
The command ID number 0x2403.
int8_t rfc_CMD_IEEE_CCA_REQ_s::currentRssi |
The RSSI currently observed on the channel.
int8_t rfc_CMD_IEEE_CCA_REQ_s::maxRssi |
The maximum RSSI observed on the channel since Rx was started.