0.01.00
Border Router

This module includes functions to manage local network data with the OpenThread Border Router. More...

Functions

OTAPI otError OTCALL otBorderRouterGetNetData (otInstance *aInstance, bool aStable, uint8_t *aData, uint8_t *aDataLength)
 This method provides a full or stable copy of the local Thread Network Data. More...
 
OTAPI otError OTCALL otBorderRouterAddOnMeshPrefix (otInstance *aInstance, const otBorderRouterConfig *aConfig)
 Add a border router configuration to the local network data. More...
 
OTAPI otError OTCALL otBorderRouterRemoveOnMeshPrefix (otInstance *aInstance, const otIp6Prefix *aPrefix)
 Remove a border router configuration from the local network data. More...
 
OTAPI otError OTCALL otBorderRouterGetNextOnMeshPrefix (otInstance *aInstance, otNetworkDataIterator *aIterator, otBorderRouterConfig *aConfig)
 This function gets the next On Mesh Prefix in the local Network Data. More...
 
OTAPI otError OTCALL otBorderRouterAddRoute (otInstance *aInstance, const otExternalRouteConfig *aConfig)
 Add an external route configuration to the local network data. More...
 
OTAPI otError OTCALL otBorderRouterRemoveRoute (otInstance *aInstance, const otIp6Prefix *aPrefix)
 Remove an external route configuration from the local network data. More...
 
OTAPI otError OTCALL otBorderRouterGetNextRoute (otInstance *aInstance, otNetworkDataIterator *aIterator, otExternalRouteConfig *aConfig)
 This function gets the next external route in the local Network Data. More...
 
OTAPI otError OTCALL otBorderRouterRegister (otInstance *aInstance)
 Immediately register the local network data with the Leader. More...
 

Detailed Description

This module includes functions to manage local network data with the OpenThread Border Router.

Function Documentation

§ otBorderRouterAddOnMeshPrefix()

OTAPI otError OTCALL otBorderRouterAddOnMeshPrefix ( otInstance aInstance,
const otBorderRouterConfig aConfig 
)

Add a border router configuration to the local network data.

Parameters
[in]aInstanceA pointer to an OpenThread instance.
[in]aConfigA pointer to the border router configuration.
Return values
OT_ERROR_NONESuccessfully added the configuration to the local network data.
OT_ERROR_INVALID_ARGSOne or more configuration parameters were invalid.
OT_ERROR_NO_BUFSNot enough room is available to add the configuration to the local network data.
See also
otBorderRouterRemoveOnMeshPrefix
otBorderRouterRegister

§ otBorderRouterAddRoute()

OTAPI otError OTCALL otBorderRouterAddRoute ( otInstance aInstance,
const otExternalRouteConfig aConfig 
)

Add an external route configuration to the local network data.

Parameters
[in]aInstanceA pointer to an OpenThread instance.
[in]aConfigA pointer to the external route configuration.
Return values
OT_ERROR_NONESuccessfully added the configuration to the local network data.
OT_ERROR_INVALID_ARGSOne or more configuration parameters were invalid.
OT_ERROR_NO_BUFSNot enough room is available to add the configuration to the local network data.
See also
otBorderRouterRemoveRoute
otBorderRouterRegister

§ otBorderRouterGetNetData()

OTAPI otError OTCALL otBorderRouterGetNetData ( otInstance aInstance,
bool  aStable,
uint8_t *  aData,
uint8_t *  aDataLength 
)

This method provides a full or stable copy of the local Thread Network Data.

Parameters
[in]aInstanceA pointer to an OpenThread instance.
[in]aStableTRUE when copying the stable version, FALSE when copying the full version.
[out]aDataA pointer to the data buffer.
[in,out]aDataLengthOn entry, size of the data buffer pointed to by aData. On exit, number of copied bytes.

§ otBorderRouterGetNextOnMeshPrefix()

OTAPI otError OTCALL otBorderRouterGetNextOnMeshPrefix ( otInstance aInstance,
otNetworkDataIterator aIterator,
otBorderRouterConfig aConfig 
)

This function gets the next On Mesh Prefix in the local Network Data.

Parameters
[in]aInstanceA pointer to an OpenThread instance.
[in,out]aIteratorA pointer to the Network Data iterator context. To get the first on-mesh entry it should be set to OT_NETWORK_DATA_ITERATOR_INIT.
[out]aConfigA pointer to the On Mesh Prefix information.
Return values
OT_ERROR_NONESuccessfully found the next On Mesh prefix.
OT_ERROR_NOT_FOUNDNo subsequent On Mesh prefix exists in the Thread Network Data.

§ otBorderRouterGetNextRoute()

OTAPI otError OTCALL otBorderRouterGetNextRoute ( otInstance aInstance,
otNetworkDataIterator aIterator,
otExternalRouteConfig aConfig 
)

This function gets the next external route in the local Network Data.

Parameters
[in]aInstanceA pointer to an OpenThread instance.
[in,out]aIteratorA pointer to the Network Data iterator context. To get the first external route entry it should be set to OT_NETWORK_DATA_ITERATOR_INIT.
[out]aConfigA pointer to the External Route information.
Return values
OT_ERROR_NONESuccessfully found the next External Route.
OT_ERROR_NOT_FOUNDNo subsequent external route entry exists in the Thread Network Data.

§ otBorderRouterRegister()

OTAPI otError OTCALL otBorderRouterRegister ( otInstance aInstance)

Immediately register the local network data with the Leader.

Parameters
[in]aInstanceA pointer to an OpenThread instance.
Return values
OT_ERROR_NONESuccessfully queued a Server Data Request message for delivery.
See also
otBorderRouterAddOnMeshPrefix
otBorderRouterRemoveOnMeshPrefix
otBorderRouterAddRoute
otBorderRouterRemoveRoute

§ otBorderRouterRemoveOnMeshPrefix()

OTAPI otError OTCALL otBorderRouterRemoveOnMeshPrefix ( otInstance aInstance,
const otIp6Prefix aPrefix 
)

Remove a border router configuration from the local network data.

Parameters
[in]aInstanceA pointer to an OpenThread instance.
[in]aPrefixA pointer to an IPv6 prefix.
Return values
OT_ERROR_NONESuccessfully removed the configuration from the local network data.
OT_ERROR_NOT_FOUNDCould not find the Border Router entry.
See also
otBorderRouterAddOnMeshPrefix
otBorderRouterRegister

§ otBorderRouterRemoveRoute()

OTAPI otError OTCALL otBorderRouterRemoveRoute ( otInstance aInstance,
const otIp6Prefix aPrefix 
)

Remove an external route configuration from the local network data.

Parameters
[in]aInstanceA pointer to an OpenThread instance.
[in]aPrefixA pointer to an IPv6 prefix.
Return values
OT_ERROR_NONESuccessfully removed the configuration from the local network data.
OT_ERROR_NOT_FOUNDCould not find the Border Router entry.
See also
otBorderRouterAddRoute
otBorderRouterRegister