Macros
Collaboration diagram for Command Codes:

Macros

#define SPICC26X2DMA_CMD_RETURN_PARTIAL_ENABLE   (SPI_CMD_RESERVED + 0)
 Command used by SPI_control to enable partial return. More...
 
#define SPICC26X2DMA_CMD_RETURN_PARTIAL_DISABLE   (SPI_CMD_RESERVED + 1)
 Command used by SPI_control to disable partial return. More...
 
#define SPICC26X2DMA_CMD_SET_CSN_PIN   (SPI_CMD_RESERVED + 2)
 Command used by SPI_control to re-configure chip select pin. More...
 
#define SPICC26XXDMA_CMD_RETURN_PARTIAL_ENABLE   (SPI_CMD_RESERVED + 0)
 Command used by SPI_control to enable partial return. More...
 
#define SPICC26XXDMA_CMD_RETURN_PARTIAL_DISABLE   (SPI_CMD_RESERVED + 1)
 Command used by SPI_control to disable partial return. More...
 
#define SPICC26XXDMA_CMD_SET_CSN_PIN   (SPI_CMD_RESERVED + 2)
 Command used by SPI_control to re-configure chip select pin. More...
 

Detailed Description

SPI_CMD_* macros are general command codes for SPI_control(). Not all SPI driver implementations support these command codes.

SPICC26X2DMA_CMD_* macros are command codes only defined in the SPICC26X2DMA.h driver implementation and need to:

#include <ti/drivers/sdspi/SPICC26X2DMA.h>

SPICC26XXDMA_CMD_* macros are command codes only defined in the SPICC26XXDMA.h driver implementation and need to:

#include <ti/drivers/sdspi/SPICC26XXDMA.h>

Macro Definition Documentation

§ SPICC26X2DMA_CMD_RETURN_PARTIAL_ENABLE

#define SPICC26X2DMA_CMD_RETURN_PARTIAL_ENABLE   (SPI_CMD_RESERVED + 0)

Command used by SPI_control to enable partial return.

Enabling this command allows SPI_transfer to return partial data if data reception is inactive for a given 32-bit period. With this command arg is don't care and it returns SPI_STATUS_SUCCESS.

§ SPICC26X2DMA_CMD_RETURN_PARTIAL_DISABLE

#define SPICC26X2DMA_CMD_RETURN_PARTIAL_DISABLE   (SPI_CMD_RESERVED + 1)

Command used by SPI_control to disable partial return.

Disabling this command returns the SPICC26X2DMA to the default blocking behavior where SPI_transfer blocks until all data bytes were received. With this comand arg is don't care and it returns SPI_STATUS_SUCCESS.

§ SPICC26X2DMA_CMD_SET_CSN_PIN

#define SPICC26X2DMA_CMD_SET_CSN_PIN   (SPI_CMD_RESERVED + 2)

Command used by SPI_control to re-configure chip select pin.

This command specifies a chip select pin With this command arg is of type PIN_Id and it return SPI_STATUS_SUCCESS

§ SPICC26XXDMA_CMD_RETURN_PARTIAL_ENABLE

#define SPICC26XXDMA_CMD_RETURN_PARTIAL_ENABLE   (SPI_CMD_RESERVED + 0)

Command used by SPI_control to enable partial return.

Enabling this command allows SPI_transfer to return partial data if data reception is inactive for a given 32-bit period. With this command arg is don't care and it returns SPI_STATUS_SUCCESS.

§ SPICC26XXDMA_CMD_RETURN_PARTIAL_DISABLE

#define SPICC26XXDMA_CMD_RETURN_PARTIAL_DISABLE   (SPI_CMD_RESERVED + 1)

Command used by SPI_control to disable partial return.

Disabling this command returns the SPICC26XXDMA to the default blocking behavior where SPI_transfer blocks until all data bytes were received. With this comand arg is don't care and it returns SPI_STATUS_SUCCESS.

§ SPICC26XXDMA_CMD_SET_CSN_PIN

#define SPICC26XXDMA_CMD_SET_CSN_PIN   (SPI_CMD_RESERVED + 2)

Command used by SPI_control to re-configure chip select pin.

This command specifies a chip select pin With this command arg is of type PIN_Id and it return SPI_STATUS_SUCCESS

© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale