SimpleLink™ CC2640R2 SDK BLE5-Stack User's Guide
1.01.15.00
  • Disclaimer
  • TI BLE5-Stack Quick Start
  • Software Architecture
  • TI-RTOS (RTOS Kernel) Overview
  • Application
  • BLE5-Stack
  • Developing a Custom Application
  • Running the SDK on Custom Hardware
  • Creating a Voice Enabled Application
  • Network Processor Interface (NPI)
  • Sensor Controller
  • Debugging
  • Memory overview
  • Updating from previous SDKs
    • Porting Guides
      • BLE5-Stack 1.01.13 (SDK 5.10) to BLE5-Stack 1.01.14 (SDK 5.30)
      • BLE5-Stack 1.01.12 (SDK 4.40) to BLE5-Stack 1.01.13 (SDK 5.10)
      • BLE5-Stack 1.01.11 (SDK 4.30) to BLE5-Stack 1.01.12 (SDK 4.40)
      • BLE5-Stack 1.01.09 (SDK 4.10) to BLE5-Stack 1.01.11 (SDK 4.30)
      • BLE5-Stack 1.01.08 (SDK 3.40) to BLE5-Stack 1.01.09 (SDK 4.10)
      • BLE5-Stack 1.01.07 (SDK 3.30) to BLE5-Stack 1.01.08 (SDK 3.40)
      • BLE5-Stack 1.01.06 (SDK 3.20) to BLE5-Stack 1.01.07 (SDK 3.30)
      • BLE5-Stack 1.01.05 (SDK 3.10) to BLE5-Stack 1.01.06 (SDK 3.20)
      • BLE5-Stack 1.01.04 (SDK 2.40) to BLE5-Stack 1.01.05 (SDK 3.10)
      • BLE5-Stack 1.01.03 (SDK 2.30) to BLE5-Stack 1.01.04 (SDK 2.40)
      • BLE5-Stack 1.01.02 (SDK 2.20) to BLE5-Stack 1.01.03 (SDK 2.30)
      • BLE5-Stack 1.01.00 to BLE5-Stack 1.01.02
      • BLE5-Stack 1.00.01 to BLE5-Stack 1.01.00
    • Year-to-Year Migration Guides
      • BLE5-Stack 1.01.09 (SDK 4.10) to BLE5-Stack 1.01.13 (SDK 5.10)
      • BLE5-Stack 1.01.08 (SDK 3.40) to BLE5-Stack 1.01.13 (SDK 5.10)
    • Migration Guides
      • Porting BLE-Stack to BLE5-Stack
      • Running Software Examples on CC2640R2L
  • API References
  • Terms and Definitions
SimpleLink™ CC2640R2 SDK BLE5-Stack User's Guide
  • »
  • Updating from previous SDKs

Updating from previous SDKs¶

Porting Guides¶

Porting guide is used to port incremental changes from the previous SDK.

  • BLE5-Stack 1.01.13 (SDK 5.10) to BLE5-Stack 1.01.14 (SDK 5.30)
  • BLE5-Stack 1.01.12 (SDK 4.40) to BLE5-Stack 1.01.13 (SDK 5.10)
  • BLE5-Stack 1.01.11 (SDK 4.30) to BLE5-Stack 1.01.12 (SDK 4.40)
  • BLE5-Stack 1.01.09 (SDK 4.10) to BLE5-Stack 1.01.11 (SDK 4.30)
  • BLE5-Stack 1.01.08 (SDK 3.40) to BLE5-Stack 1.01.09 (SDK 4.10)
  • BLE5-Stack 1.01.07 (SDK 3.30) to BLE5-Stack 1.01.08 (SDK 3.40)
  • BLE5-Stack 1.01.06 (SDK 3.20) to BLE5-Stack 1.01.07 (SDK 3.30)
  • BLE5-Stack 1.01.05 (SDK 3.10) to BLE5-Stack 1.01.06 (SDK 3.20)
  • BLE5-Stack 1.01.04 (SDK 2.40) to BLE5-Stack 1.01.05 (SDK 3.10)
  • BLE5-Stack 1.01.03 (SDK 2.30) to BLE5-Stack 1.01.04 (SDK 2.40)
  • BLE5-Stack 1.01.02 (SDK 2.20) to BLE5-Stack 1.01.03 (SDK 2.30)
  • BLE5-Stack 1.01.00 to BLE5-Stack 1.01.02
  • BLE5-Stack 1.00.01 to BLE5-Stack 1.01.00
  • BLE5-Stack 1.00.00 to BLE5-Stack 1.00.01

Year-to-Year Migration Guides¶

The following migration guides are designed to help migrate across multiple SDK releases.

  • BLE5-Stack 1.01.09 (SDK 4.10) to BLE5-Stack 1.01.13 (SDK 5.10)
  • BLE5-Stack 1.01.08 (SDK 3.40) to BLE5-Stack 1.01.13 (SDK 5.10)

Migration Guides¶

Migration guide is used to migrate major changes from one device to another device.

  • Porting BLE-Stack to BLE5-Stack
  • Running Software Examples on CC2640R2L
  • CC2640 to CC2640R2F

  • CC254x to CC2640

Previous Next

© Copyright 2010-2024, Texas Instruments.