BLE5-Stack 1.00.00 to BLE5-Stack 1.00.01ΒΆ
This section will describe a way to migrate a project from BLE5-Stack 1.00.00 to a BLE5-Stack 1.00.01 project.
For this migration guide, simple_peripheral from BLE5-Stack 1.00.00 will be ported over to BLE5-Stack 1.00.01. Because the directory structure is nearly identical between the two releases, the recommended approach is to start with a BLE5-Stack 1.00.01 project that contains the same base functionality as the porting target project and merge in any custom functionality.
Choose a BLE5-Stack 1.00.01 example project that contains your target project’s base functionality.
For reference, see available sample projects that start with simple_
In this example, we’re going to use simple_peripheral as the starting BLE5-Stack 1.00.01 sample project.
Transfer all modified application files from BLE5-Stack 1.00.00 into the BLE5-Stack 1.00.01 example project.
In this example, the following files from BLE5-Stack 1.00.00 were moved into simple_peripheral BLE5-Stack 1.00.01 example:
simple_peripheral.csimple_peripheral.hsimple_gatt_profile.csimple_gatt_profile.h
If your code contains any
#ifdef USE_CORE_SDK, remove these.Modify
main.cin the BLE5-Stack 1.00.01 example if additional tasks were added in the BLE5-Stack 1.00.00 project.Please do not add any
DV42_FEATURESdefines tobuild_config.optin BLE5-Stack 1.00.01. If you want to enable or disable sec-secure-connections, please use the GAPBOND_SECURE_CONNECTION parameter. (Secure Connections is enabled by default in BLE5-Stack 1.00.01.)uint8_t gapbondSecure = GAPBOND_SECURE_CONNECTION_NONE; GAPBondMgr_SetParameter(GAPBOND_SECURE_CONNECTION, sizeof(uint8_t), &gapbondSecure);
In BLE-Stack BLE5-Stack 1.00.01, heap management has been updated. Please see Dynamic Memory Allocation for details on how to optimize your heap.
If you are using the GAPBondMgr, make sure a passcode callback function is defined and sent to the GAPBondMgr. This is mandatory in BLE5-Stack 1.00.01.
// GAP Bond Manager Callbacks // These are set to NULL since they are not needed. The application // is set up to only perform justworks pairing. static gapBondCBs_t simpleBLEPeripheral_BondMgrCBs = { (pfnPasscodeCB_t) SimpleBLEPeripheral_passcodeCB, // Passcode callback SimpleBLEPeripheral_pairStateCB // Pairing / Bonding state Callback };
The passcode can be defined as follows:
/********************************************************************* * @fn SimpleBLEPeripheral_passcodeCB * * @brief Passcode callback. * * @return none */ static void SimpleBLEPeripheral_passcodeCB(uint8_t *deviceAddr, uint16_t connHandle, uint8_t uiInputs, uint8_t uiOutputs) { uint8_t *pData; // Allocate space for the passcode event. if ((pData = ICall_malloc(sizeof(uint8_t)))) { *pData = uiOutputs; // Enqueue the event. SimpleBLEPeripheral_enqueueMsg(SBP_PASSCODE_NEEDED_EVT, 0, pData); } }
If necessary, update the project to use the newer TI-RTOS drivers that are supplied with the SimpleLink CC2640R2 SDK.
The following drivers have changed from BLE5-Stack 1.00.00. Please see the changes to these drivers by comparing the supplied headers between those in simplelink_cc2640r2_sdk_1_30_00_25 and those in the SimpleLink CC2640R2 SDK.
ADCNVSDisplay
Attention
The display folder should in BLE5-Stack 1.00.01 be included with the path
<ti/display/Display.h>, not<ti/mw/display/Display.h>.#include <ti/display/Display.h>
Refer to the Upgrade and Compatibility Information for additional information and the TI-RTOS examples included with SimpleLink CC2640R2 SDK.
For additional information on how BLE5-Stack 1.00.01 uses TI-RTOS see TI-RTOS Overview
For any utilized TI Drivers, review `TI-RTOS Kernel Users Guide`_ and Driver APIs.