Data Fields
LCD_Config Struct Reference

The LCD_Config structure contains a set of pointers used to characterize the LCD driver implementation. More...

#include <LCDDogm1286.h>

Collaboration diagram for LCD_Config:
Collaboration graph
[legend]

Data Fields

LCD_Objectobject
 
LCD_HWAttrs const * hwAttrs
 

Detailed Description

The LCD_Config structure contains a set of pointers used to characterize the LCD driver implementation.

Field Documentation

§ object

LCD_Object* LCD_Config::object

Pointer to a driver specific data object

§ hwAttrs

LCD_HWAttrs const* LCD_Config::hwAttrs

Pointer to a driver specific hardware attributes structure


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale