Data Fields
ECJPAKECC26X2_Object_ Struct Reference

ECJPAKECC26X2 Object. More...

#include <ECJPAKECC26X2.h>

Collaboration diagram for ECJPAKECC26X2_Object_:
Collaboration graph
[legend]

Data Fields

bool isOpen
 
bool operationInProgress
 
bool operationCanceled
 
int_fast16_t operationStatus
 
ECJPAKE_CallbackFxn callbackFxn
 
ECJPAKE_ReturnBehavior returnBehavior
 
ECJPAKECC26X2_FsmState fsmState
 
ECJPAKE_Operation operation
 
ECJPAKE_OperationType operationType
 
uint32_t semaphoreTimeout
 
uint32_t resultAddress
 

Detailed Description

ECJPAKECC26X2 Object.

The application must not access any member variables of this structure!

Field Documentation

§ isOpen

bool ECJPAKECC26X2_Object_::isOpen

§ operationInProgress

bool ECJPAKECC26X2_Object_::operationInProgress

§ operationCanceled

bool ECJPAKECC26X2_Object_::operationCanceled

§ operationStatus

int_fast16_t ECJPAKECC26X2_Object_::operationStatus

§ callbackFxn

ECJPAKE_CallbackFxn ECJPAKECC26X2_Object_::callbackFxn

§ returnBehavior

ECJPAKE_ReturnBehavior ECJPAKECC26X2_Object_::returnBehavior

§ fsmState

ECJPAKECC26X2_FsmState ECJPAKECC26X2_Object_::fsmState

§ operation

ECJPAKE_Operation ECJPAKECC26X2_Object_::operation

§ operationType

ECJPAKE_OperationType ECJPAKECC26X2_Object_::operationType

§ semaphoreTimeout

uint32_t ECJPAKECC26X2_Object_::semaphoreTimeout

§ resultAddress

uint32_t ECJPAKECC26X2_Object_::resultAddress

The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale