Data Fields
ADCCC26XX_Object Struct Reference

ADCCC26XX Object. More...

#include <ADCCC26XX.h>

Collaboration diagram for ADCCC26XX_Object:
Collaboration graph
[legend]

Data Fields

PIN_State pinState
 
PIN_Handle pinHandle
 
bool isOpen
 
bool isProtected
 

Detailed Description

ADCCC26XX Object.

The application must not access any member variables of this structure!

Field Documentation

§ pinState

PIN_State ADCCC26XX_Object::pinState

Pin state object

§ pinHandle

PIN_Handle ADCCC26XX_Object::pinHandle

Pin handle

§ isOpen

bool ADCCC26XX_Object::isOpen

Flag if the instance is in use

§ isProtected

bool ADCCC26XX_Object::isProtected

Flag to indicate if thread safety is ensured by the driver


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale