Data Structures | Typedefs | Functions | Variables
DisplayDogm1286.h File Reference
#include <ti/drivers/dpl/SemaphoreP.h>
#include <ti/drivers/SPI.h>
#include <ti/display/Display.h>
#include <ti/display/lcd/LCDDogm1286.h>
#include <stdint.h>
Include dependency graph for DisplayDogm1286.h:

Go to the source code of this file.

Data Structures

struct  DisplayDogm1286_HWAttrs
 
struct  DisplayDogm1286_Object
 

Typedefs

typedef struct DisplayDogm1286_HWAttrs DisplayDogm1286_HWAttrs
 
typedef struct DisplayDogm1286_Object DisplayDogm1286_Object
 
typedef struct DisplayDogm1286_ObjectDisplayDogm1286_Handle
 

Functions

void DisplayDogm1286_init (Display_Handle handle)
 
Display_Handle DisplayDogm1286_open (Display_Handle, Display_Params *params)
 
void DisplayDogm1286_clear (Display_Handle handle)
 
void DisplayDogm1286_clearLines (Display_Handle handle, uint8_t fromLine, uint8_t toLine)
 
void DisplayDogm1286_vprintf (Display_Handle handle, uint8_t line, uint8_t column, char *fmt, va_list va)
 
void DisplayDogm1286_close (Display_Handle)
 
int DisplayDogm1286_control (Display_Handle handle, unsigned int cmd, void *arg)
 
unsigned int DisplayDogm1286_getType (void)
 

Variables

const Display_FxnTable DisplayDogm1286_fxnTable
 

Typedef Documentation

§ DisplayDogm1286_HWAttrs

§ DisplayDogm1286_Object

§ DisplayDogm1286_Handle

Function Documentation

§ DisplayDogm1286_init()

void DisplayDogm1286_init ( Display_Handle  handle)

§ DisplayDogm1286_open()

Display_Handle DisplayDogm1286_open ( Display_Handle  ,
Display_Params params 
)

§ DisplayDogm1286_clear()

void DisplayDogm1286_clear ( Display_Handle  handle)

§ DisplayDogm1286_clearLines()

void DisplayDogm1286_clearLines ( Display_Handle  handle,
uint8_t  fromLine,
uint8_t  toLine 
)

§ DisplayDogm1286_vprintf()

void DisplayDogm1286_vprintf ( Display_Handle  handle,
uint8_t  line,
uint8_t  column,
char *  fmt,
va_list  va 
)

§ DisplayDogm1286_close()

void DisplayDogm1286_close ( Display_Handle  )

§ DisplayDogm1286_control()

int DisplayDogm1286_control ( Display_Handle  handle,
unsigned int  cmd,
void *  arg 
)

§ DisplayDogm1286_getType()

unsigned int DisplayDogm1286_getType ( void  )

Variable Documentation

§ DisplayDogm1286_fxnTable

const Display_FxnTable DisplayDogm1286_fxnTable
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale