CC26xx Driver Library
rfc_CMD_SET_TX_POWER_s Struct Reference

Set Transmit Power. More...

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0010. More...
 
uint16_t txPower
 New TX power setting Bits 0–5: IB Value to write to the PA power control field at 25 °C Bits 6–7: GC Value to write to the gain control of the 1st stage of the PA Bits 8–15: tempCoeff Temperature coefficient for IB. 0: No temperature compensation. More...
 

Detailed Description

Set Transmit Power.

Field Documentation

uint16_t rfc_CMD_SET_TX_POWER_s::commandNo

The command ID number 0x0010.

uint16_t rfc_CMD_SET_TX_POWER_s::txPower

New TX power setting Bits 0–5: IB Value to write to the PA power control field at 25 °C Bits 6–7: GC Value to write to the gain control of the 1st stage of the PA Bits 8–15: tempCoeff Temperature coefficient for IB. 0: No temperature compensation.