CC26xx Driver Library
rfc_CMD_PROP_RX_s Struct Reference

Proprietary Mode Receive Command. More...

#include <rf_prop_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x3802. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More...
 
condition
 
struct {
   uint8_t   bFsOff:1
 0: Keep frequency synth on after command
1: Turn frequency synth off after command More...
 
   uint8_t   bRepeatOk:1
 0: End operation after receiving a packet correctly
1: Go back to sync search after receiving a packet correctly More...
 
   uint8_t   bRepeatNok:1
 0: End operation after receiving a packet with CRC error
1: Go back to sync search after receiving a packet with CRC error More...
 
   uint8_t   bUseCrc:1
 0: Do not check CRC
1: Check CRC More...
 
   uint8_t   bVarLen:1
 0: Fixed length
1: Receive length as first byte More...
 
   uint8_t   bChkAddress:1
 0: No address check
1: Check address More...
 
   uint8_t   endType:1
 0: Packet is received to the end if end trigger happens after sync is obtained
1: Packet reception is stopped if end trigger happens More...
 
   uint8_t   filterOp:1
 0: Stop receiver and restart sync search on address mismatch
1: Receive packet and mark it as ignored on address mismatch More...
 
pktConf
 
struct {
   uint8_t   bAutoFlushIgnored:1
 If 1, automatically discard ignored packets from RX queue. More...
 
   uint8_t   bAutoFlushCrcErr:1
 If 1, automatically discard packets with CRC error from RX queue. More...
 
   uint8_t   __pad0__:1
 
   uint8_t   bIncludeHdr:1
 If 1, include the received header or length byte in the stored packet; otherwise discard it. More...
 
   uint8_t   bIncludeCrc:1
 If 1, include the received CRC field in the stored packet; otherwise discard it. More...
 
   uint8_t   bAppendRssi:1
 If 1, append an RSSI byte to the packet in the RX queue. More...
 
   uint8_t   bAppendTimestamp:1
 If 1, append a timestamp to the packet in the RX queue. More...
 
   uint8_t   bAppendStatus:1
 If 1, append a status byte to the packet in the RX queue. More...
 
rxConf
 RX configuration. More...
 
uint32_t syncWord
 Sync word to listen for. More...
 
uint8_t maxPktLen
 Packet length for fixed length, maximum packet length for variable length
0: Unlimited or unknown length. More...
 
uint8_t address0
 Address. More...
 
uint8_t address1
 Address (set equal to address0 to accept only one address. If 0xFF, accept 0x00 as well) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
endTrigger
 Trigger classifier for ending the operation. More...
 
ratmr_t endTime
 Time used together with endTrigger for ending the operation. More...
 
dataQueue_tpQueue
 Pointer to receive queue. More...
 
uint8_t * pOutput
 Pointer to output structure. More...
 

Detailed Description

Proprietary Mode Receive Command.

Field Documentation

uint8_t rfc_CMD_PROP_RX_s::__pad0__
uint8_t rfc_CMD_PROP_RX_s::address0

Address.

uint8_t rfc_CMD_PROP_RX_s::address1

Address (set equal to address0 to accept only one address. If 0xFF, accept 0x00 as well)

uint8_t rfc_CMD_PROP_RX_s::bAppendRssi

If 1, append an RSSI byte to the packet in the RX queue.

uint8_t rfc_CMD_PROP_RX_s::bAppendStatus

If 1, append a status byte to the packet in the RX queue.

uint8_t rfc_CMD_PROP_RX_s::bAppendTimestamp

If 1, append a timestamp to the packet in the RX queue.

uint8_t rfc_CMD_PROP_RX_s::bAutoFlushCrcErr

If 1, automatically discard packets with CRC error from RX queue.

uint8_t rfc_CMD_PROP_RX_s::bAutoFlushIgnored

If 1, automatically discard ignored packets from RX queue.

uint8_t rfc_CMD_PROP_RX_s::bChkAddress

0: No address check
1: Check address

uint8_t rfc_CMD_PROP_RX_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

uint8_t rfc_CMD_PROP_RX_s::bFsOff

0: Keep frequency synth on after command
1: Turn frequency synth off after command

uint8_t rfc_CMD_PROP_RX_s::bIncludeCrc

If 1, include the received CRC field in the stored packet; otherwise discard it.

uint8_t rfc_CMD_PROP_RX_s::bIncludeHdr

If 1, include the received header or length byte in the stored packet; otherwise discard it.

uint8_t rfc_CMD_PROP_RX_s::bRepeatNok

0: End operation after receiving a packet with CRC error
1: Go back to sync search after receiving a packet with CRC error

uint8_t rfc_CMD_PROP_RX_s::bRepeatOk

0: End operation after receiving a packet correctly
1: Go back to sync search after receiving a packet correctly

uint8_t rfc_CMD_PROP_RX_s::bUseCrc

0: Do not check CRC
1: Check CRC

uint8_t rfc_CMD_PROP_RX_s::bVarLen

0: Fixed length
1: Receive length as first byte

uint16_t rfc_CMD_PROP_RX_s::commandNo

The command ID number 0x3802.

struct { ... } rfc_CMD_PROP_RX_s::condition
ratmr_t rfc_CMD_PROP_RX_s::endTime

Time used together with endTrigger for ending the operation.

struct { ... } rfc_CMD_PROP_RX_s::endTrigger

Trigger classifier for ending the operation.

uint8_t rfc_CMD_PROP_RX_s::endType

0: Packet is received to the end if end trigger happens after sync is obtained
1: Packet reception is stopped if end trigger happens

uint8_t rfc_CMD_PROP_RX_s::filterOp

0: Stop receiver and restart sync search on address mismatch
1: Receive packet and mark it as ignored on address mismatch

uint8_t rfc_CMD_PROP_RX_s::maxPktLen

Packet length for fixed length, maximum packet length for variable length
0: Unlimited or unknown length.

uint8_t rfc_CMD_PROP_RX_s::nSkip

Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...

uint8_t rfc_CMD_PROP_RX_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

struct { ... } rfc_CMD_PROP_RX_s::pktConf
rfc_radioOp_t* rfc_CMD_PROP_RX_s::pNextOp

Pointer to the next operation to run after this operation is done.

uint8_t* rfc_CMD_PROP_RX_s::pOutput

Pointer to output structure.

dataQueue_t* rfc_CMD_PROP_RX_s::pQueue

Pointer to receive queue.

uint8_t rfc_CMD_PROP_RX_s::rule

Condition for running next command: Rule for how to proceed.

struct { ... } rfc_CMD_PROP_RX_s::rxConf

RX configuration.

ratmr_t rfc_CMD_PROP_RX_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

struct { ... } rfc_CMD_PROP_RX_s::startTrigger

Identification of the trigger that starts the operation.

uint16_t rfc_CMD_PROP_RX_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

uint32_t rfc_CMD_PROP_RX_s::syncWord

Sync word to listen for.

uint8_t rfc_CMD_PROP_RX_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

uint8_t rfc_CMD_PROP_RX_s::triggerType

The type of trigger.