|
void | SetupTrimDevice (void) |
| Performs the necessary trim of the device which is not done in ROM boot code. More...
|
|
This module contains functions for device setup which is not done in boot code.
void SetupTrimDevice |
( |
void |
| ) |
|
Performs the necessary trim of the device which is not done in ROM boot code.
This function should only execute coming from ROM boot.
The following is handled by this function:
- Checks if the driverlib variant used by the application is supported by the device. Execution is halted in case of unsupported driverlib variant.
- Configures VIMS cache mode based on setting in CCFG.
- Configures functionalities like DCDC and XOSC dependent on startup modes like cold reset, wakeup from shutdown and wakeup from from powerdown.
- Configures VIMS power domain control.
- Configures optimal wait time for flash FSM in cases where flash pump wakes up from sleep.
- Note
- The current implementation does not take soft reset into account. However, it does no damage to execute it again. It only consumes time.
-
This function is called by the compiler specific device startup codes that are integrated in the SimpleLink SDKs for CC13xx/CC26XX devices.
- Returns
- None
110 uint32_t ui32Fcfg1Revision;
111 uint32_t ui32AonSysResetctl;
116 if ( ui32Fcfg1Revision == 0xFFFFFFFF ) {
117 ui32Fcfg1Revision = 0;
141 NOROM_SetupSetCacheModeAccordingToCcfgSetting();
void ThisLibraryIsFor_CC26x0R2_HaltIfViolated(void)
Verifies that current chip is CC26x0R2 and never returns if violated.
Definition: chipinfo.c:169
static void TrimAfterColdResetWakeupFromShutDownWakeupFromPowerDown(void)
Trims to be applied when coming from POWER_DOWN (also called when coming from SHUTDOWN and PIN_RESET)...
Definition: setup.c:231
static void TrimAfterColdResetWakeupFromShutDown(uint32_t ui32Fcfg1Revision)
Trims to be applied when coming from SHUTDOWN (also called when coming from PIN_RESET).
Definition: setup.c:247
void SetupSetCacheModeAccordingToCcfgSetting(void)
Set correct VIMS_MODE according to CCFG setting (CACHE or GPRAM)
Definition: setup_rom.c:837
static void TrimAfterColdReset(void)
Trims to be applied when coming from PIN_RESET.
Definition: setup.c:336