CC26xx Driver Library
aux_adc.c File Reference
#include "aux_adc.h"
#include "../inc/hw_memmap.h"
#include "../inc/hw_aux_wuc.h"
#include "../inc/hw_fcfg1.h"
#include "adi.h"
#include "event.h"

Functions

void AUXADCDisable (void)
 Disables the ADC. More...
 
void AUXADCEnableAsync (uint32_t refSource, uint32_t trigger)
 Enables the ADC for asynchronous operation. More...
 
void AUXADCEnableSync (uint32_t refSource, uint32_t sampleTime, uint32_t trigger)
 Enables the ADC for synchronous operation. More...
 
void AUXADCDisableInputScaling (void)
 Disables scaling of the ADC input. More...
 
void AUXADCFlushFifo (void)
 Flushes the ADC FIFO. More...
 
uint32_t AUXADCReadFifo (void)
 Waits for and returns the first sample in the ADC FIFO. More...
 
uint32_t AUXADCPopFifo (void)
 Returns the first sample in the ADC FIFO, without waiting. More...
 
int32_t AUXADCGetAdjustmentGain (uint32_t refSource)
 Returns the gain value used when adjusting for ADC gain/offset. More...
 
int32_t AUXADCGetAdjustmentOffset (uint32_t refSource)
 Returns the offset value used when adjusting for ADC gain/offset. More...
 
int32_t AUXADCValueToMicrovolts (int32_t fixedRefVoltage, int32_t adcValue)
 Converts an "adjusted" ADC value to microvolts. More...
 
int32_t AUXADCMicrovoltsToValue (int32_t fixedRefVoltage, int32_t microvolts)
 Converts a number of microvolts to corresponding "adjusted" ADC value. More...
 
int32_t AUXADCAdjustValueForGainAndOffset (int32_t adcValue, int32_t gain, int32_t offset)
 Performs ADC value gain and offset adjustment. More...
 
int32_t AUXADCUnadjustValueForGainAndOffset (int32_t adcValue, int32_t gain, int32_t offset)
 Performs the inverse of the ADC value gain and offset adjustment. More...