|
#define | SNP_BLE_GAP_BOND_REJECTED bleGAPBondRejected |
| 0x32, General status, The bound information was rejected.
|
|
#define | SNP_BLE_MEM_ALLOC_ERROR bleMemAllocError |
| 0x13, General status, Memory allocation error occurred
|
|
#define | SNP_BLE_NO_RESOURCES bleNoResources |
| 0x15, General status, There are no resource available
|
|
#define | SNP_BLE_TIMEOUT bleTimeout |
| 0x17, General status, Timed out performing function
|
|
#define | SNP_INVALIDPARAMETER INVALIDPARAMETER |
| 0x2, General status, Invalid Parameter
|
|
#define | SNP_LL_CTRL_PKT_TIMEOUT_TERM LL_CTRL_PKT_TIMEOUT_TERM |
| 0x22, LL status, Link Layer Response Timeout
|
|
#define | SNP_LL_ENC_KEY_REQ_REJECTED LL_ENC_KEY_REQ_REJECTED |
| 0x06, LL status, Pin or Key Missing
|
|
#define | SNP_LL_ENC_KEY_REQ_UNSUPPORTED_FEATURE LL_ENC_KEY_REQ_UNSUPPORTED_FEATURE |
| 0x1A, LL status, Unsupported Remote Feature
|
|
#define | SNP_LL_STATUS_ERROR_BAD_PARAMETER LL_STATUS_ERROR_BAD_PARAMETER |
| 0x12, LL status, Invalid HCI Command Parameters or 0x30: Parameter Out of Mandatory Range?
|
|
#define | SNP_LL_STATUS_ERROR_COMMAND_DISALLOWED LL_STATUS_ERROR_COMMAND_DISALLOWED |
| 0x0C, LL status, Command Disallowed
|
|
#define | SNP_LL_STATUS_ERROR_CTRL_PROC_ALREADY_ACTIVE LL_STATUS_ERROR_CTRL_PROC_ALREADY_ACTIVE |
| 0x3A, LL status, Controller Busy
|
|
#define | SNP_LL_STATUS_ERROR_FEATURE_NOT_SUPPORTED LL_STATUS_ERROR_FEATURE_NOT_SUPPORTED |
| 0x11, LL status, Unsupported Feature or Parameter Value
|
|
#define | SNP_LL_STATUS_ERROR_INACTIVE_CONNECTION LL_STATUS_ERROR_INACTIVE_CONNECTION |
| 0x02, LL status, Unknown Connection Identifier for now; may be needed for multiple connections
|
|
#define | SNP_SMP_PAIRING_FAILED_AUTH_REQ SMP_PAIRING_FAILED_AUTH_REQ |
| 0x03, SMP status, The pairing procedure can't be performed as authentication requirements can't be met due to IO capabilities of one or both devices
|
|
#define | SNP_SMP_PAIRING_FAILED_CMD_NOT_SUPPORTED SMP_PAIRING_FAILED_CMD_NOT_SUPPORTED |
| 0x07, SMP status, The SMP command received is not supported on this device.
|
|
#define | SNP_SMP_PAIRING_FAILED_CONFIRM_VALUE SMP_PAIRING_FAILED_CONFIRM_VALUE |
| 0x04, SMP status, The confirm value doesn't match the calculated compare value
|
|
#define | SNP_SMP_PAIRING_FAILED_DHKEY_CHECK_FAILED SMP_PAIRING_FAILED_DHKEY_CHECK_FAILED |
| 0x0B, SMP status, Indicates to the remote device that the DHKey Check value received does not match the one calculated by the local device.
|
|
#define | SNP_SMP_PAIRING_FAILED_ENC_KEY_SIZE SMP_PAIRING_FAILED_ENC_KEY_SIZE |
| 0x06, SMP status, The resultant encryption key size is insufficient for the security requirements of this device.
|
|
#define | SNP_SMP_PAIRING_FAILED_NOT_SUPPORTED SMP_PAIRING_FAILED_NOT_SUPPORTED |
| 0x05, SMP status, Pairing isn't supported by the device
|
|
#define | SNP_SMP_PAIRING_FAILED_NUM_COMPARISON_FAILED SMP_PAIRING_FAILED_NUM_COMPARISON_FAILED |
| 0x0C, SMP status, Indicates that the confirm value in the numeric comparison protocol do not match.
|
|
#define | SNP_SMP_PAIRING_FAILED_OOB_NOT_AVAIL SMP_PAIRING_FAILED_OOB_NOT_AVAIL |
| 0x02, SMP status, The OOB data is not available
|
|
#define | SNP_SMP_PAIRING_FAILED_PASSKEY_ENTRY_FAILED SMP_PAIRING_FAILED_PASSKEY_ENTRY_FAILED |
| 0x01, SMP status, The user input of the passkey failed, for example, the user cancelled the operation.
|
|
#define | SNP_SMP_PAIRING_FAILED_UNSPECIFIED SMP_PAIRING_FAILED_UNSPECIFIED |
| 0x08, SMP status, Pairing failed due to an unspecified reason
|
|
List of GENERAL status codes that are transfered to the SAP layer. Note: These defines were added after the SAP was not able to understand the statuses that were transfered "as is" to the pGapBondCB->pairStateCB. The values of these defines is copied from the original define status.