TI BLE5-Stack API Documentation  1.01.14.00
Data Fields
hciEvt_BLEDataLengthChange_t Struct Reference

LE Data Length Change Event. More...

Data Fields

uint8 BLEEventCode
 BLE Event Code.
 
uint16 connHandle
 connection handle
 
osal_event_hdr_t hdr
 osal event header
 
uint16 maxRxOctets
 maximum receive bytes
 
uint16 maxRxTime
 maximum receive time
 
uint16 maxTxOctets
 maximum transmission bytes
 
uint16 maxTxTime
 maximum transmission time
 

Detailed Description

LE Data Length Change Event.


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale